![]() |
0.01.00
|
This file defines the OpenThread Server API. More...
#include <openthread/types.h>Go to the source code of this file.
Functions | |
| OTAPI otError OTCALL | otServerGetNetDataLocal (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength) |
| This method provides a full or stable copy of the local Thread Network Data. More... | |
| OTAPI otError OTCALL | otServerAddService (otInstance *aInstance, const otServiceConfig *aConfig) |
| Add a service configuration to the local network data. More... | |
| OTAPI otError OTCALL | otServerRemoveService (otInstance *aInstance, uint32_t aEnterpriseNumber, uint8_t *aServiceData, uint8_t aServiceDataLength) |
| Remove a service configuration from the local network data. More... | |
| OTAPI otError OTCALL | otServerGetNextService (otInstance *aInstance, otNetworkDataIterator *aIterator, otServiceConfig *aConfig) |
| This function gets the next service in the local Network Data. More... | |
| OTAPI otError OTCALL | otServerRegister (otInstance *aInstance) |
| Immediately register the local network data with the Leader. More... | |
This file defines the OpenThread Server API.