This module includes functions to manage local network data with the OpenThread Server.
More...
This module includes functions to manage local network data with the OpenThread Server.
§ otServerAddService()
Add a service configuration to the local network data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aConfig | A pointer to the service configuration. |
- Return values
-
| OT_ERROR_NONE | Successfully added the configuration to the local network data. |
| OT_ERROR_INVALID_ARGS | One or more configuration parameters were invalid. |
| OT_ERROR_NO_BUFS | Not enough room is available to add the configuration to the local network data. |
- See also
- otServerRemoveService
-
otServerRegister
§ otServerGetNetDataLocal()
This method provides a full or stable copy of the local Thread Network Data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aStable | TRUE when copying the stable version, FALSE when copying the full version. |
| [out] | aData | A pointer to the data buffer. |
| [in,out] | aDataLength | On entry, size of the data buffer pointed to by aData. On exit, number of copied bytes. |
§ otServerGetNextService()
This function gets the next service in the local Network Data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first service entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to where the service information will be placed. |
- Return values
-
| OT_ERROR_NONE | Successfully found the next service. |
| OT_ERROR_NOT_FOUND | No subsequent service exists in the Thread Network Data. |
§ otServerRegister()
Immediately register the local network data with the Leader.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Return values
-
| OT_ERROR_NONE | Successfully queued a Server Data Request message for delivery. |
- See also
- otServerAddService
-
otServerRemoveService
§ otServerRemoveService()
| OTAPI otError OTCALL otServerRemoveService |
( |
otInstance * |
aInstance, |
|
|
uint32_t |
aEnterpriseNumber, |
|
|
uint8_t * |
aServiceData, |
|
|
uint8_t |
aServiceDataLength |
|
) |
| |
Remove a service configuration from the local network data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aEnterpriseNumber | Enterprise Number of the service entry to be deleted. |
| [in] | aServiceData | A pointer to an Service Data to look for during deletion. |
| [in] | aServiceDataLength | The length of aServiceData in bytes. |
- Return values
-
| OT_ERROR_NONE | Successfully removed the configuration from the local network data. |
| OT_ERROR_NOT_FOUND | Could not find the Border Router entry. |
- See also
- otServerAddService
-
otServerRegister