![]() |
0.01.00
|
This file defines the OpenThread Network Data API. More...
#include <openthread/types.h>Go to the source code of this file.
Functions | |
| OTAPI otError OTCALL | otNetDataGet (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength) |
| This method provides a full or stable copy of the Leader's Thread Network Data. More... | |
| OTAPI otError OTCALL | otNetDataGetNextOnMeshPrefix (otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig) |
| This function gets the next On Mesh Prefix in the partition's Network Data. More... | |
| otError | otNetDataGetNextRoute (otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig) |
| This function gets the next external route in the partition's Network Data. More... | |
| OTAPI uint8_t OTCALL | otNetDataGetVersion (otInstance *aInstance) |
| Get the Network Data Version. More... | |
| OTAPI uint8_t OTCALL | otNetDataGetStableVersion (otInstance *aInstance) |
| Get the Stable Network Data Version. More... | |
This file defines the OpenThread Network Data API.