This module includes the platform abstraction for the message pool.
More...
This module includes the platform abstraction for the message pool.
§ otPlatMessagePoolFree()
This function is used to free a Buffer back to the platform managed buffer pool.
- Parameters
-
| [in] | aInstance | A pointer to the OpenThread instance. |
| [in] | aBuffer | The Buffer to free. |
§ otPlatMessagePoolInit()
| void otPlatMessagePoolInit |
( |
otInstance * |
aInstance, |
|
|
uint16_t |
aMinNumFreeBuffers, |
|
|
size_t |
aBufferSize |
|
) |
| |
Initialize the platform implemented message pool.
- Parameters
-
| [in] | aInstance | A pointer to the OpenThread instance. |
| [in] | aMinNumFreeBuffers | An uint16 containing the minimum number of free buffers desired by OpenThread. |
| [in] | aBufferSize | The size in bytes of a Buffer object. |
§ otPlatMessagePoolNew()
Allocate a buffer from the platform managed buffer pool.
- Parameters
-
| [in] | aInstance | A pointer to the OpenThread instance. |
- Returns
- A pointer to the Buffer or NULL if no Buffers are available.
§ otPlatMessagePoolNumFreeBuffers()
| uint16_t otPlatMessagePoolNumFreeBuffers |
( |
otInstance * |
aInstance | ) |
|
Get the number of free buffers.
- Parameters
-
| [in] | aInstance | A pointer to the OpenThread instance. |
- Returns
- The number of buffers currently free and available to OpenThread.