![]() |
0.01.00
|
This file implements the OpenThread Tasklet API. More...
#include "openthread-core-config.h"#include <openthread/tasklet.h>#include "openthread-instance.h"#include "common/code_utils.hpp"#include "common/logging.hpp"Macros | |
| #define | WPP_NAME "tasklet_api.tmh" |
Functions | |
| void | otTaskletsProcess (otInstance *aInstance) |
| Run all queued OpenThread tasklets at the time this is called. More... | |
| bool | otTaskletsArePending (otInstance *aInstance) |
| Indicates whether or not OpenThread has tasklets pending. More... | |
| OT_TOOL_WEAK void | otTaskletsSignalPending (otInstance *) |
| OpenThread calls this function when the tasklet queue transitions from empty to non-empty. More... | |
This file implements the OpenThread Tasklet API.