This module includes functions that control the Thread stack's execution.
More...
This module includes functions that control the Thread stack's execution.
§ otTaskletsArePending()
| bool otTaskletsArePending |
( |
otInstance * |
aInstance | ) |
|
Indicates whether or not OpenThread has tasklets pending.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
- Return values
-
| TRUE | If there are tasklets pending. |
| FALSE | If there are no tasklets pending. |
§ otTaskletsProcess()
Run all queued OpenThread tasklets at the time this is called.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
§ otTaskletsSignalPending()
| void otTaskletsSignalPending |
( |
otInstance * |
aInstance | ) |
|
OpenThread calls this function when the tasklet queue transitions from empty to non-empty.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |