This module includes the platform abstraction for diagnostics features.
More...
This module includes the platform abstraction for diagnostics features.
§ otPlatDiagAlarmCallback()
| void otPlatDiagAlarmCallback |
( |
otInstance * |
aInstance | ) |
|
This function processes the alarm event.
- Parameters
-
| [in] | aInstance | The OpenThread instance for current request. |
§ otPlatDiagChannelSet()
| void otPlatDiagChannelSet |
( |
uint8_t |
aChannel | ) |
|
This function sets the channel to use for factory diagnostics.
- Parameters
-
| [in] | aChannel | The channel value. |
§ otPlatDiagModeGet()
| bool otPlatDiagModeGet |
( |
void |
| ) |
|
This function indicates whether or not factory diagnostics mode is enabled.
- Returns
- TRUE if factory diagnostics mode is enabled, FALSE otherwise.
§ otPlatDiagModeSet()
| void otPlatDiagModeSet |
( |
bool |
aMode | ) |
|
This function enables/disables the factory diagnostics mode.
- Parameters
-
| [in] | aMode | TRUE to enable diagnostics mode, FALSE otherwise. |
§ otPlatDiagProcess()
| void otPlatDiagProcess |
( |
otInstance * |
aInstance, |
|
|
int |
argc, |
|
|
char * |
argv[], |
|
|
char * |
aOutput, |
|
|
size_t |
aOutputMaxLen |
|
) |
| |
This function processes a factory diagnostics command line.
- Parameters
-
| [in] | aInstance | The OpenThread instance for current request. |
| [in] | argc | The argument counter of diagnostics command line. |
| [in] | argv | The argument vector of diagnostics command line. |
| [out] | aOutput | The diagnostics execution result. |
| [in] | aOutputMaxLen | The output buffer size. |
§ otPlatDiagRadioReceived()
This function processes the received radio frame.
- Parameters
-
| [in] | aInstance | The OpenThread instance for current request. |
| [in] | aFrame | The received radio frame. |
| [in] | aError | The received radio frame status. |
§ otPlatDiagTxPowerSet()
| void otPlatDiagTxPowerSet |
( |
int8_t |
aTxPower | ) |
|
This function sets the transmit power to use for factory diagnostics.
- Parameters
-
| [in] | aTxPower | The transmit power value. |