This module includes the platform abstraction for the alarm service.
More...
This module includes the platform abstraction for the alarm service.
§ otPlatAlarmMicroFired()
| void otPlatAlarmMicroFired |
( |
otInstance * |
aInstance | ) |
|
Signal that the alarm has fired.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
§ otPlatAlarmMicroGetNow()
| uint32_t otPlatAlarmMicroGetNow |
( |
void |
| ) |
|
Get the current time.
- Returns
- The current time in microseconds.
§ otPlatAlarmMicroStartAt()
| void otPlatAlarmMicroStartAt |
( |
otInstance * |
aInstance, |
|
|
uint32_t |
aT0, |
|
|
uint32_t |
aDt |
|
) |
| |
Set the alarm to fire at aDt microseconds after aT0.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aT0 | The reference time. |
| [in] | aDt | The time delay in microseconds from aT0. |
§ otPlatAlarmMicroStop()
| void otPlatAlarmMicroStop |
( |
otInstance * |
aInstance | ) |
|
Stop the alarm.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
§ otPlatAlarmMilliFired()
| void otPlatAlarmMilliFired |
( |
otInstance * |
aInstance | ) |
|
Signal that the alarm has fired.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
§ otPlatAlarmMilliGetNow()
| uint32_t otPlatAlarmMilliGetNow |
( |
void |
| ) |
|
Get the current time.
- Returns
- The current time in milliseconds.
§ otPlatAlarmMilliStartAt()
| void otPlatAlarmMilliStartAt |
( |
otInstance * |
aInstance, |
|
|
uint32_t |
aT0, |
|
|
uint32_t |
aDt |
|
) |
| |
Set the alarm to fire at aDt milliseconds after aT0.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aT0 | The reference time. |
| [in] | aDt | The time delay in milliseconds from aT0. |
§ otPlatAlarmMilliStop()
| void otPlatAlarmMilliStop |
( |
otInstance * |
aInstance | ) |
|
Stop the alarm.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
§ otPlatDiagAlarmFired()
| void otPlatDiagAlarmFired |
( |
otInstance * |
aInstance | ) |
|
Signal diagnostics module that the alarm has fired.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |