This file defines the top-level functions for the OpenThread CoAP implementation.
More...
|
| enum | otCoapType {
OT_COAP_TYPE_CONFIRMABLE = 0x00,
OT_COAP_TYPE_NON_CONFIRMABLE = 0x10,
OT_COAP_TYPE_ACKNOWLEDGMENT = 0x20,
OT_COAP_TYPE_RESET = 0x30
} |
| | CoAP Type values. More...
|
| |
| enum | otCoapCode {
OT_COAP_CODE_EMPTY = OT_COAP_CODE(0, 0),
OT_COAP_CODE_GET = OT_COAP_CODE(0, 1),
OT_COAP_CODE_POST = OT_COAP_CODE(0, 2),
OT_COAP_CODE_PUT = OT_COAP_CODE(0, 3),
OT_COAP_CODE_DELETE = OT_COAP_CODE(0, 4),
OT_COAP_CODE_RESPONSE_MIN = OT_COAP_CODE(2, 0),
OT_COAP_CODE_CREATED = OT_COAP_CODE(2, 1),
OT_COAP_CODE_DELETED = OT_COAP_CODE(2, 2),
OT_COAP_CODE_VALID = OT_COAP_CODE(2, 3),
OT_COAP_CODE_CHANGED = OT_COAP_CODE(2, 4),
OT_COAP_CODE_CONTENT = OT_COAP_CODE(2, 5),
OT_COAP_CODE_BAD_REQUEST = OT_COAP_CODE(4, 0),
OT_COAP_CODE_UNAUTHORIZED = OT_COAP_CODE(4, 1),
OT_COAP_CODE_BAD_OPTION = OT_COAP_CODE(4, 2),
OT_COAP_CODE_FORBIDDEN = OT_COAP_CODE(4, 3),
OT_COAP_CODE_NOT_FOUND = OT_COAP_CODE(4, 4),
OT_COAP_CODE_METHOD_NOT_ALLOWED = OT_COAP_CODE(4, 5),
OT_COAP_CODE_NOT_ACCEPTABLE = OT_COAP_CODE(4, 6),
OT_COAP_CODE_PRECONDITION_FAILED = OT_COAP_CODE(4, 12),
OT_COAP_CODE_REQUEST_TOO_LARGE = OT_COAP_CODE(4, 13),
OT_COAP_CODE_UNSUPPORTED_FORMAT = OT_COAP_CODE(4, 15),
OT_COAP_CODE_INTERNAL_ERROR = OT_COAP_CODE(5, 0),
OT_COAP_CODE_NOT_IMPLEMENTED = OT_COAP_CODE(5, 1),
OT_COAP_CODE_BAD_GATEWAY = OT_COAP_CODE(5, 2),
OT_COAP_CODE_SERVICE_UNAVAILABLE = OT_COAP_CODE(5, 3),
OT_COAP_CODE_GATEWAY_TIMEOUT = OT_COAP_CODE(5, 4),
OT_COAP_CODE_PROXY_NOT_SUPPORTED = OT_COAP_CODE(5, 5)
} |
| | CoAP Code values. More...
|
| |
| enum | otCoapOptionType {
OT_COAP_OPTION_IF_MATCH = 1,
OT_COAP_OPTION_URI_HOST = 3,
OT_COAP_OPTION_E_TAG = 4,
OT_COAP_OPTION_IF_NONE_MATCH = 5,
OT_COAP_OPTION_OBSERVE = 6,
OT_COAP_OPTION_URI_PORT = 7,
OT_COAP_OPTION_LOCATION_PATH = 8,
OT_COAP_OPTION_URI_PATH = 11,
OT_COAP_OPTION_CONTENT_FORMAT = 12,
OT_COAP_OPTION_MAX_AGE = 14,
OT_COAP_OPTION_URI_QUERY = 15,
OT_COAP_OPTION_ACCEPT = 17,
OT_COAP_OPTION_LOCATION_QUERY = 20,
OT_COAP_OPTION_PROXY_URI = 35,
OT_COAP_OPTION_PROXY_SCHEME = 39,
OT_COAP_OPTION_SIZE1 = 60
} |
| | CoAP Option Numbers. More...
|
| |
| enum | otCoapOptionContentFormat {
OT_COAP_OPTION_CONTENT_FORMAT_TEXT_PLAIN = 0,
OT_COAP_OPTION_CONTENT_FORMAT_LINK_FORMAT = 40,
OT_COAP_OPTION_CONTENT_FORMAT_XML = 41,
OT_COAP_OPTION_CONTENT_FORMAT_OCTET_STREAM = 42,
OT_COAP_OPTION_CONTENT_FORMAT_EXI = 47,
OT_COAP_OPTION_CONTENT_FORMAT_JSON = 50
} |
| | CoAP Content Format codes. More...
|
| |
|
| void | otCoapHeaderInit (otCoapHeader *aHeader, otCoapType aType, otCoapCode aCode) |
| | This function initializes the CoAP header. More...
|
| |
| void | otCoapHeaderSetToken (otCoapHeader *aHeader, const uint8_t *aToken, uint8_t aTokenLength) |
| | This function sets the Token value and length in a header. More...
|
| |
| void | otCoapHeaderGenerateToken (otCoapHeader *aHeader, uint8_t aTokenLength) |
| | This function sets the Token length and randomizes its value. More...
|
| |
| otError | otCoapHeaderAppendContentFormatOption (otCoapHeader *aHeader, otCoapOptionContentFormat aContentFormat) |
| | This function appends the Content Format CoAP option as specified in https://tools.ietf.org/html/rfc7252#page-92. More...
|
| |
| otError | otCoapHeaderAppendOption (otCoapHeader *aHeader, const otCoapOption *aOption) |
| | This function appends a CoAP option in a header. More...
|
| |
| otError | otCoapHeaderAppendUintOption (otCoapHeader *aHeader, uint16_t aNumber, uint32_t aValue) |
| | This function appends an unsigned integer CoAP option as specified in https://tools.ietf.org/html/rfc7252#section-3.2. More...
|
| |
| otError | otCoapHeaderAppendObserveOption (otCoapHeader *aHeader, uint32_t aObserve) |
| | This function appends an Observe option. More...
|
| |
| otError | otCoapHeaderAppendUriPathOptions (otCoapHeader *aHeader, const char *aUriPath) |
| | This function appends an Uri-Path option. More...
|
| |
| otError | otCoapHeaderAppendMaxAgeOption (otCoapHeader *aHeader, uint32_t aMaxAge) |
| | This function appends a Max-Age option. More...
|
| |
| otError | otCoapHeaderAppendUriQueryOption (otCoapHeader *aHeader, const char *aUriQuery) |
| | This function appends a single Uri-Query option. More...
|
| |
| void | otCoapHeaderSetPayloadMarker (otCoapHeader *aHeader) |
| | This function adds Payload Marker indicating beginning of the payload to the CoAP header. More...
|
| |
| void | otCoapHeaderSetMessageId (otCoapHeader *aHeader, uint16_t aMessageId) |
| | This function sets the Message ID value. More...
|
| |
| otCoapType | otCoapHeaderGetType (const otCoapHeader *aHeader) |
| | This function returns the Type value. More...
|
| |
| otCoapCode | otCoapHeaderGetCode (const otCoapHeader *aHeader) |
| | This function returns the Code value. More...
|
| |
| uint16_t | otCoapHeaderGetMessageId (const otCoapHeader *aHeader) |
| | This function returns the Message ID value. More...
|
| |
| uint8_t | otCoapHeaderGetTokenLength (const otCoapHeader *aHeader) |
| | This function returns the Token length. More...
|
| |
| const uint8_t * | otCoapHeaderGetToken (const otCoapHeader *aHeader) |
| | This function returns a pointer to the Token value. More...
|
| |
| const otCoapOption * | otCoapHeaderGetFirstOption (otCoapHeader *aHeader) |
| | This function returns a pointer to the first option. More...
|
| |
| const otCoapOption * | otCoapHeaderGetNextOption (otCoapHeader *aHeader) |
| | This function returns a pointer to the next option. More...
|
| |
| otMessage * | otCoapNewMessage (otInstance *aInstance, const otCoapHeader *aHeader) |
| | This function creates a new message with a CoAP header. More...
|
| |
| otError | otCoapSendRequest (otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext) |
| | This function sends a CoAP request. More...
|
| |
| otError | otCoapStart (otInstance *aInstance, uint16_t aPort) |
| | This function starts the CoAP server. More...
|
| |
| otError | otCoapStop (otInstance *aInstance) |
| | This function stops the CoAP server. More...
|
| |
| otError | otCoapAddResource (otInstance *aInstance, otCoapResource *aResource) |
| | This function adds a resource to the CoAP server. More...
|
| |
| void | otCoapRemoveResource (otInstance *aInstance, otCoapResource *aResource) |
| | This function removes a resource from the CoAP server. More...
|
| |
| void | otCoapSetDefaultHandler (otInstance *aInstance, otCoapRequestHandler aHandler, void *aContext) |
| | This function sets the default handler for unhandled CoAP requests. More...
|
| |
| otError | otCoapSendResponse (otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo) |
| | This function sends a CoAP response from the server. More...
|
| |
This file defines the top-level functions for the OpenThread CoAP implementation.