This module includes the platform abstraction for radio configuration.
More...
This module includes the platform abstraction for radio configuration.
§ otPlatRadioGetIeeeEui64()
| void otPlatRadioGetIeeeEui64 |
( |
otInstance * |
aInstance, |
|
|
uint8_t * |
aIeeeEui64 |
|
) |
| |
Get the factory-assigned IEEE EUI-64 for this interface.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [out] | aIeeeEui64 | A pointer to the factory-assigned IEEE EUI-64. |
§ otPlatRadioSetExtendedAddress()
Set the Extended Address for address filtering.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aExtAddress | A pointer to the IEEE 802.15.4 Extended Address stored in little-endian byte order. |
§ otPlatRadioSetPanId()
| void otPlatRadioSetPanId |
( |
otInstance * |
aInstance, |
|
|
uint16_t |
aPanId |
|
) |
| |
Set the PAN ID for address filtering.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aPanId | The IEEE 802.15.4 PAN ID. |
§ otPlatRadioSetShortAddress()
| void otPlatRadioSetShortAddress |
( |
otInstance * |
aInstance, |
|
|
uint16_t |
aShortAddress |
|
) |
| |
Set the Short Address for address filtering.
- Parameters
-
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aShortAddress | The IEEE 802.15.4 Short Address. |