![]() |
![]() |
SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
![]() |
Macros | |
#define | SD_STATUS_SUCCESS (0) |
Successful status code returned by SD_control(). More... | |
#define | SD_STATUS_ERROR (-1) |
Generic error status code returned by SD_control(). More... | |
#define | SD_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SD_control() for undefined command codes. More... | |
SD_STATUS_* macros are general status codes returned by SD_control()
#define SD_STATUS_SUCCESS (0) |
Successful status code returned by SD_control().
SD_control() returns SD_STATUS_SUCCESS if the control code was executed successfully.
#define SD_STATUS_ERROR (-1) |
Generic error status code returned by SD_control().
SD_control() returns SD_STATUS_ERROR if the control code was not executed successfully.
#define SD_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SD_control() for undefined command codes.
SD_control() returns SD_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.