TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapPasskeyNeededEvent_t Struct Reference

GAP_PASSKEY_NEEDED_EVENT message format. More...

Data Fields

uint16 connectionHandle
 Connection handle.
 
uint8 deviceAddr [B_ADDR_LEN]
 address of device to pair with, and could be either public or random.
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint32 numComparison
 Numeric Comparison value to be displayed.
 
uint8 opcode
 GAP_PASSKEY_NEEDED_EVENT
 
uint8 uiInputs
 Pairing User Interface Inputs - Ask user to input passcode.
 
uint8 uiOutputs
 Pairing User Interface Outputs - Display passcode.
 

Detailed Description

GAP_PASSKEY_NEEDED_EVENT message format.

This message is sent to the app when a Passkey is needed from the app's user interface.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated