TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapDeviceInitDoneEvent_t Struct Reference

GAP_DEVICE_INIT_DONE_EVENT message format. More...

Data Fields

uint16 dataPktLen
 HC_LE_Data_Packet_Length.
 
uint8 devAddr [B_ADDR_LEN]
 Device's BD_ADDR.
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint8 numDataPkts
 HC_Total_Num_LE_Data_Packets.
 
uint8 opcode
 GAP_DEVICE_INIT_DONE_EVENT
 

Detailed Description

GAP_DEVICE_INIT_DONE_EVENT message format.

This message is sent to the app when the Device Initialization is done [initiated by calling GAP_DeviceInit()].


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated