TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapDeviceInfoEvent_t Struct Reference

GAP_DEVICE_INFO_EVENT message format. More...

Data Fields

uint8 addr [B_ADDR_LEN]
 Address of the advertisement or SCAN_RSP.
 
uint8 addrType
 address type: Address Types
 
uint8 dataLen
 Length (in bytes) of the data field (evtData)
 
uint8 eventType
 Advertisement Type: GAP Advertising Report Event Types.
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint8 opcode
 GAP_DEVICE_INFO_EVENT
 
uint8 * pEvtData
 Data field of advertisement or SCAN_RSP.
 
int8 rssi
 Advertisement or SCAN_RSP RSSI.
 

Detailed Description

GAP_DEVICE_INFO_EVENT message format.

This message is sent to the app during a Device Discovery Request, when a new advertisement or scan response is received.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated