TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapBondCompleteEvent_t Struct Reference

GAP_BOND_COMPLETE_EVENT message format. More...

Data Fields

uint16 connectionHandle
 connection Handle
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint8 opcode
 GAP_BOND_COMPLETE_EVENT
 

Detailed Description

GAP_BOND_COMPLETE_EVENT message format.

This message is sent to the app when a bonding is complete. This means that a key is loaded and the link is encrypted.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated