Docker Setup for ROS 2¶
In the ROS 2 Docker images both for TDA4 and Ubuntu PC, following two popular DDS implementations are installed:
eProsima Fast DDS (default DDS for ROS 2 Foxy)
Eclipse Cyclone DDS (additionally installed)
To make the out-of-box demos run smooth, the following DDS selection are made in the ROS 2 Docker containers by default on each platform.
| Platform | DDS Choice | Note |
|---|---|---|
| TDA4 target | Eclipse Cyclone DDS | Provides better performance, especially with "rosbag play" |
| Visualization PC | eProsima Fast DDS | Provides better Ctrl+C response |
By setting an environment variable RMW_IMPLEMENTATION you can switch the DDS implementation in each launch session. For example,
To use eProsima Fast DDS,
RMW_IMPLEMENTATION=rmw_fastrtps_cpp ros2 ...
To use Eclipse Cyclone DDS,
RMW_IMPLEMENTATION=rmw_cyclonedds_cpp ros2 ...
1. Set Up Docker Environment on the TDA4¶
In ROS 2 Docker container environment, ROS Foxy and necessary libraries and tools are installed.
To generate the scripts for building and running a Docker image for ROS 2 Foxy:
root@tda4vm-sk:~/j7ros_home$ make scripts ROS_VER=2
Please make sure that two bash scripts,
docker_build_ros2.shanddocker_run_ros2.sh, are generated.To build the Docker image:
root@tda4vm-sk:~/j7ros_home$ ./docker_build_ros2.sh
This step will take several minutes depending on the network speed, and once “docker build” is completed, you can check the resulting Docker image with
docker images.To start/run the Docker container:
root@tda4vm-sk:~/j7ros_home$ ./docker_run_ros2.sh
It is important to use
docker_run_ros2.shscript to start a Docker container, since the script includes all the necessary settings to leverage all the cores and hardware accelerators of the TDA4 device.To build the ROS applications, inside the Docker container:
root@j7-docker:~/j7ros_home/ros_ws$ colcon build --base-paths /opt/robotics_sdk/ros2 --executor sequential root@j7-docker:~/j7ros_home/ros_ws$ source install/setup.bash
The ROSBAG data downloaded is in ROS 1 specific format and the format and storage mechanism has changed in ROS 2. For converting the ROS 1 bag data to ROS 2 format, use
rosbags-convert <ros1_bag_name.bag>. This will create a directory <ros_bag_name> and contains the data under this directory. To convert the downloaded ROSBAG file, run the following inside the ROS 2 Docker container.root@j7-docker:~/j7ros_home$ rosbags-convert $WORK_DIR/data/ros_bag/zed1_2020-11-09-18-01-08.bag
2. Set Up Docker Environment on the Remote PC for Visualization¶
You can choose any folder, but init_setip.sh script sets up ${HOME}/j7ros_home as the working directory.
To generate bash scripts for building and running a Docker image for ROS 2 Foxy:
user@pc:~/j7ros_home$ make scripts ROS_VER=2
If the Ubuntu PC uses a Nvidia GPU driver, please add one more argument
GPUS=y:user@pc:~/j7ros_home$ make scripts ROS_VER=2 GPUS=y
Make sure that two bash scripts,
docker_build_ros2.shanddocker_run_ros2.sh, are generated.To build the ROS 2 Docker image:
user@pc:~/j7ros_home$ ./docker_build_ros2.sh
It will take several minutes to build the Docker image. The Docker image built can be listed with
docker images.Run the ROS 2 Docker container:
user@pc:~/j7ros_home$ ./docker_run_ros2.sh
Build the ROS nodes for visualization:
root@pc-docker:~/j7ros_home/ros_ws$ colcon build --base-paths src/robotics_sdk/ros2 root@pc-docker:~/j7ros_home/ros_ws$ source install/setup.bash
3. Run Demo Applications¶
Table below summarizes the launch commands that you can use in the Docker container for each demo, on the TDA4/J7, and on the remote visualization PC. For more details, see the following subsections.
| Demo (Input Source) | Launch command on TDA4 | Launch command on Remote Visualization PC |
|---|---|---|
| Stereo Vision (ZED camera) | ros2 launch ti_sde zed_sde_launch.py zed_sn:=SNxxxxx | ros2 launch ti_viz_nodes rviz_sde_launch.py |
| Stereo Vision with point-cloud (ZED camera) | ros2 launch ti_sde zed_sde_pcl_launch.py zed_sn:=SNxxxxx | ros2 launch ti_viz_nodes rviz_sde_pcl_launch.py |
| Semantic Segmentation CNN (ZED camera) | ros2 launch ti_vision_cnn zed_semseg_cnn_launch.py zed_sn:=SNxxxxx | ros2 launch ti_viz_nodes rviz_semseg_cnn_launch.py |
| Semantic Segmentation CNN (Mono camera) | ros2 launch ti_vision_cnn gscam_semseg_cnn_launch.py | same as above |
| Object Detection CNN (ZED camera) | ros2 launch ti_vision_cnn zed_objdet_cnn_launch.py zed_sn:=SNxxxxx | ros2 launch ti_viz_nodes rviz_objdet_cnn_launch.py |
| Object Detection CNN (Mono camera) | ros2 launch ti_vision_cnn gscam_objdet_cnn_launch.py | same as above |
| 3D Obstacle Detection (ZED camera) | ros2 launch ti_estop zed_estop_launch.py zed_sn:=SNxxxxx | ros2 launch ti_viz_nodes rviz_estop_launch.py |
Running Demos with ROSBAG
It is recommended to launch demos in two terminals on the TDA4 target, and launch ros2 bag play in a separate terminal as shown in the following table.
| Demo | ROSBAG launch command on TDA4 (Terminal 1) | Demo launch command on TDA4 (Terminal 2) | Launch command on Remote Visualization PC |
|---|---|---|---|
| Stereo Vision | ros2 launch ti_sde rosbag_launch.py | ros2 launch ti_sde sde_launch.py | ros2 launch ti_viz_nodes rviz_sde_launch.py |
| Stereo Vision with point-cloud | ros2 launch ti_sde rosbag_launch.py | ros2 launch ti_sde sde_pcl_launch.py | ros2 launch ti_viz_nodes rviz_sde_pcl_launch.py |
| Semantic Segmentation CNN | ros2 launch ti_sde rosbag_remap_launch.py | ros2 launch ti_vision_cnn semseg_cnn_launch.py | ros2 launch ti_viz_nodes rviz_semseg_cnn_launch.py |
| Object Detection CNN | ros2 launch ti_sde rosbag_remap_launch.py | ros2 launch ti_vision_cnn objdet_cnn_launch.py | ros2 launch ti_viz_nodes rviz_objdet_cnn_launch.py |
| 3D Obstacle Detection | ros2 launch ti_sde rosbag_launch.py | ros2 launch ti_estop estop_launch.py | ros2 launch ti_viz_nodes rviz_estop_launch.py |
You can use TMUX inside the ROS Docker container to split the current terminal window into multiple panes. Below are some of useful basic keys in using TMUX. Full list of keys can be found, e.g., in this link.
tmux: start a tmux sessionCtrl + b, followed by": split pane verticallyCtrl + b, followed by↑or↓: switch to pane to the directionCtrl + b, followed byx: close the current pane
In the following, [TDA4] and [PC] indicate where the step(s) should be launched: either on the TDA4 target, or on the PC.
3.1. Run Stereo Vision Application¶
[TDA4] To launch
ti_sdenode with a ZED stereo camera, run the following launch command inside the ROS 2 container:root@j7-docker:~/j7ros_home/ros_ws$ ros2 launch ti_sde zed_sde_launch.py
Alternatively, you can run the following directly on the TDA4 host Linux:
root@tda4vm-sk:~/j7ros_home$ ./docker_run_ros2.sh ros2 launch ti_sde zed_sde_launch.py
[PC] For visualization, in the ROS 2 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ ros2 launch ti_viz_nodes rviz_sde_launch.py
3.2. Run Stereo Vision Application with Point-Cloud Enabled¶
[TDA4] To launch
ti_sdenode with point-cloud enabled on a ZED camera, run the following launch command inside the ROS 2 container:root@j7-docker:~/j7ros_home/ros_ws$ ros2 launch ti_sde zed_sde_pcl_launch.py
Alternatively, you can run the following directly on the TDA4 host Linux:
root@tda4vm-sk:~/j7ros_home$ ./docker_run_ros2.sh ros2 launch ti_sde zed_sde_pcl_launch.py
[PC] For visualization, in the ROS 2 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ ros2 launch ti_viz_nodes rviz_sde_pcl_launch.py
3.3. Run Semantic Segmentation CNN Application¶
[TDA4] To launch semantic segmentation demo with a ZED stereo camera, run the following launch command inside the ROS 2 container:
root@j7-docker:~/j7ros_home/ros_ws$ ros2 launch ti_vision_cnn zed_semseg_cnn_launch.py
Alternatively, you can run the following directly on the TDA4 host Linux:
root@tda4vm-sk:~/j7ros_home$ ./docker_run_ros2.sh ros2 launch ti_vision_cnn zed_semseg_cnn_launch.py
To process the image stream from a USB mono camera, replace the launch file with
gscam_semseg_cnn_launch.pyin the above.[PC] For visualization, in the ROS 2 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ ros2 launch ti_viz_nodes rviz_semseg_cnn_launch.py
3.4. Run Object Detection CNN Application¶
[TDA4] To launch object detection demo with a ZED stereo camera, run the following launch command inside the ROS 2 container:
root@tda4vm-sk:~/j7ros_home$ ./docker_run_ros2.sh ros2 launch ti_vision_cnn zed_objdet_cnn_launch.py
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-docker:~/j7ros_home/ros_ws$ ros2 launch ti_vision_cnn zed_objdet_cnn_launch.py
To process the image stream from a USB mono camera, replace the launch file with
gscam_objdet_cnn_launch.pyin the above.[PC] For visualization, in the ROS 2 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ ros2 launch ti_viz_nodes rviz_objdet_cnn_launch.py
3.5. Run 3D Obstacle Detection Application¶
[TDA4] To launch
ti_estopnode with a ZED stereo camera, run the following launch command inside the ROS 2 container:root@tda4vm-sk:~/j7ros_home$ ./docker_run_ros2.sh ros2 launch ti_estop zed_estop_launch.py
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-docker:~/j7ros_home/ros_ws$ ros2 launch ti_estop zed_estop_launch.py
[PC] For visualization, in the ROS 2 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ ros2 launch ti_viz_nodes rviz_estop_launch.py