Robotics SDK¶
Overview¶
The Jacinto Robotics SDK provides software development environment on the latest TDA4 class of SoCs, and also provides software building blocks and example demos that can be leveraged in robotics software development. The SDK runs in Docker container environments on Processor SDK Linux for Edge AI 8.4.0. We provide detailed steps for setting up Docker container environments for ROS Noetic and ROS 2 Foxy on the Processor SDK Linux for Edge AI (see next section). The Robotics SDK allows:
Optimized software implementation of computation-intensive software blocks (including deep-learning, vision, perception, mapping and localization) on deep-learning core (C7x/MMA), DSP cores, hardware accelerators built-in on the TDA4 processors.
Application software development on the target using APIs optimized on the TDA4 cores and hardware accelerators along with many open-source libraries and packages including, for example, OpenCV, Point-Cloud Library (PCL), and many more.
Figure 1 shows the software libraries and components that the Robotics SDK provides.

TI Vision Apps Library¶
TI Vision Apps Library is included in the pre-built base image for the Processor SDK Linux for Edge AI. The library provides a set of APIs including:
TI OpenVX kernels and software infrastructure
Imaging and vision applications
Perception applications
Advanced driver-assistance systems (ADAS) applications
Open-Source Deep-Learning Runtime¶
The Processor SDK Linux for Edge AI also supports the following open-source deep-learning runtime:
TVM/Neo-AI-DLR
TFLite Runtime
ONNX Runtime
For more details on open-source deep-learning runtime on TDA4x, please check TI Edge AI Cloud. The Robotics SDK provides a versatile vision CNN node optimized on TDA4x that supports many deep-learning models for object detection and semantic segmentation operations.
Figure 2 shows a representative deep-learning and compute-intensive demo application developed with the Robotics SDK.
Setting Up Robotics SDK Docker Container Environment¶
This section describes how to set up the Robotics SDK on top of the Processor SDK Linux for Edge AI. Check out our Setting Up Robotics SDK to get started.
Note: git.ti.com has some issue in rendering markdown files. We highly recommend to use the section in the User Guide Documentation
Sensor Driver Nodes¶
Following ROS nodes for cameras are tested and supported by the SDK.
Demo Applications¶
The SDK supports following out-of-box demo applications.
Scope of Robotics SDK¶

Limitations and Known Issues¶
See known_issues.md
Change Log¶
See CHANGELOG.md