Setting Up Robotics Kit Environment¶
1. Requirements & Dependency¶
Supported Hardware Platforms¶
| Platform | Supported Devices | Supported EVM |
|---|---|---|
| J721E | TDA4VM | TDA4VMXEVM |
J7 Processor SDK RTOS¶
The Robotics SDK requires the pre-built package of J721E Processor SDK RTOS 7.3.0. The pre-built package contains Processor SDK Linux and libraries that are necessary for setting up the Robotics development environment.
Ubuntu PC¶
A Ubuntu (18.04 recommended) PC is required. For RViz visualization of ROS topics published from the J7 target, it is assumed that ROS (Melodic recommended) is installed on the PC. For ROS installation steps, please refer to this ROS wiki page.
USB Stereo Camera [Optional]¶
The Robotics SDK provides a OpenCV-based ROS driver for ZED stereo camera. All the demo applications can be tried out with a live stereo camera as well as a ROSBAG file provided. For configuration of a stereo camera, please see drivers/zed_capture/README.md.
2. Set Up the J7 Target and Development Environment¶
Figure 1 shows the hardware setup and high-level installation steps on the J7 target and the Ubuntu PC.
Build SD Card¶
From Ubuntu PC, download Processor SDK RTOS 7.3.0 pre-built package
Install the pre-built package to a SD card (minimum 32GB high-performance) by referring to the instruction on this page
Connect Remotely to the J7 Target¶
To find the IP address assigned to J7 EVM, use a serial port communications program (for example,
sudo minicom -D /dev/ttyUSBxwhere/dev/ttyUSBxis the device for the UART serial port), log in withrootaccount, and runifconfig.From a terminal on the PC, open a SSH session to connect remotely to the J7 target:
user@pc:~$ ssh root@<J7_IP_address>
Note: It is recommended to use a static IP for the J7 EVM to make ROS network setting easy.
Clone Git Repository¶
Set up the project directory and the catkin workspace:
root@j7-evm:~$ WORK_DIR=$HOME/j7ros_home root@j7-evm:~$ CATKIN_WS=$WORK_DIR/catkin_ws root@j7-evm:~$ mkdir -p $CATKIN_WS/src root@j7-evm:~$ cd $CATKIN_WS/src
Clone the project GIT repository:
git clone https://git.ti.com/git/processor-sdk-vision/jacinto_ros_perception.git
Download TIDL Model & ROSBAG File¶
For convenience, set up a soft-link:
root@j7-evm:~/j7ros_home/catkin_ws/src$ cd $WORK_DIR root@j7-evm:~/j7ros_home$ ln -s $CATKIN_WS/src/jacinto_ros_perception/docker/Makefile
To download data files, run the following in
$WORK_DIR:root@j7-evm:~/j7ros_home$ make data_download
Two tarballs (for deep-learning model artifacts, and a ROSBAG file) are downloaded and uncompressed under
$WORK_DIR/data. If preferred, each tarball can be downloaded individually withmake model_downloadandmake rosbag_download, respectively.
Set Up Docker Environment¶
Following this link, check that Docker and network work correctly on the J7 host Linux.
To generate bash scripts for building and running a Docker image for the Robotics Kit:
root@j7-evm:~/j7ros_home$ make scripts
Make sure that two bash scripts,
docker_build.shanddocker_run.sh, are generated.Note: The default Dockerfile installs
ros-perceptionROS package group in the Docker image. In case you want to minimize the size of Docker image by installing only minimal dependency required to build and run the ROS nodes under$CATKIN_WS/src, use the scripts generated with the following:root@j7-evm:~/j7ros_home$ make scripts_rosdep
To build the Docker image, in
$WORK_DIRrun:root@j7-evm:~/j7ros_home$ ./docker_build.sh
It will take several minutes to build the Docker image. The Docker image built can be listed with
docker images.
3. Set Up the Ubuntu PC for Visualization¶
Open another terminal on Ubuntu PC to set up environment for RViz visualization.
Clone the GIT repository:
user@pc:~$ CATKIN_WS=$HOME/j7ros_home/catkin_ws user@pc:~$ mkdir -p $CATKIN_WS/src user@pc:~$ cd $CATKIN_WS/src git clone https://git.ti.com/git/processor-sdk-vision/jacinto_ros_perception.git
Build the ROS nodes for visualization:
user@pc:~/j7ros_home/catkin_ws/src$ cd $CATKIN_WS user@pc:~/j7ros_home/catkin_ws$ catkin_make
ROS network setting: For convenience, set up a soft-link:
user@pc:~/j7ros_home/catkin_ws$ ln -s src/jacinto_ros_perception/setup_env_pc.sh
Update the following lines in
setup_env_pc.sh:PC_IP_ADDR=<PC_IP_address> J7_IP_ADDR=<J7_IP_address>
<J7_IP_address>can be found by runningmake ip_showon a J7 terminal.To set up the PC environment, run the following:
user@pc:~/j7ros_home/catkin_ws$ source setup_env_pc.sh
4. Build and Run Demo Applications¶
Build the ROS Applications¶
To run the Docker image:
root@j7-evm:~/j7ros_home$ ./docker_run.sh
To build the ROS applications, inside the Docker container:
root@j7-docker:~/j7ros_home/catkin_ws$ catkin_make root@j7-docker:~/j7ros_home/catkin_ws$ source devel/setup.bash
Run Stereo Vision Application¶
[J7] To launch
ti_sdenode with playing back a ROSBAG file, run the following in$WORK_DIRon the J7 host Linux:root@j7-evm:~/j7ros_home$ ./docker_run.sh roslaunch ti_sde bag_sde.launch
Alternatively, you can run the following
roslaunchcommand inside the Docker container:root@j7-docker:~/j7ros_home/catkin_ws$ roslaunch ti_sde bag_sde.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_sde.launchin the above.[PC] For visualization, on the PC:
user@pc:~/j7ros_home/catkin_ws$ roslaunch ti_sde rviz.launch
Run Stereo Vision Application with Point-Cloud Enabled¶
[J7] To launch
ti_sdenode with playing back a ROSBAG file, run the following in$WORK_DIRon the J7 host Linux:root@j7-evm:~/j7ros_home$ ./docker_run.sh roslaunch ti_sde bag_sde_pcl.launch
Alternatively, you can run the following
roslaunchcommand inside the Docker container:root@j7-docker:~/j7ros_home/catkin_ws$ roslaunch ti_sde bag_sde_pcl.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_sde.launchin the above.[PC] For visualization, on the PC (Make sure
source setup_env_pc.shahead):user@pc:~/j7ros_home/catkin_ws$ roslaunch ti_sde rviz_pcl.launch
Run CNN Semantic Segmentation Application¶
[J7] To launch
ti_semseg_cnnnode with playing back a ROSBAG file, run the following in$WORK_DIRon the J7 host Linux:root@j7-evm:~/j7ros_home$ ./docker_run.sh roslaunch ti_semseg_cnn bag_semseg_cnn.launch
Alternatively, you can run the following
roslaunchcommand inside the Docker container:root@j7-docker:~/j7ros_home/catkin_ws$ roslaunch ti_semseg_cnn bag_semseg_cnn.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_semseg_cnn.launchin the above.[PC] For visualization, on the PC:
user@pc:~/j7ros_home/catkin_ws$ roslaunch ti_semseg_cnn rviz.launch
Run 3D Obstacle Detection Application¶
[J7] To launch
ti_estopnode with playing back a ROSBAG file, run the following in$WORK_DIRon the J7 host Linux:root@j7-evm:~/j7ros_home$ ./docker_run.sh roslaunch ti_estop bag_estop.launch
Alternatively, you can run the following
roslaunchcommand inside the Docker container:root@j7-docker:~/j7ros_home/catkin_ws$ roslaunch ti_estop bag_estop.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_estop.launchin the above.[PC] For visualization, on the PC:
user@pc:~/j7ros_home/catkin_ws$ roslaunch ti_estop rviz.launch