TIOVX User Guide
|
Implementation of Graph object. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_parameters_t |
The list of graph parameters. More... | |
struct | tivx_data_ref_q_list_t |
The list of data refs other than graph parameters. More... | |
struct | tivx_delay_data_ref_q_list_t |
The list of delay data refs other than graph parameters. More... | |
struct | tivx_graph_t |
The top level data for graph object. More... | |
Macros | |
#define | TIVX_DEFAULT_GRAPH_TIMEOUT (TIVX_EVENT_TIMEOUT_WAIT_FOREVER) |
Default timeout value for graph level control event ACK waits. This is the default timeout value used within the following APIs. More... | |
#define | TIVX_GRAPH_PARAMETER_ENQUEUE_FLAG_PIPEUP (0x00000001u) |
Flag used with tivxGraphParameterEnqueueReadyRef to indicate that this enqueue call if for pipeup phase. More... | |
Functions | |
int32_t | ownGraphGetFreeNodeIndex (vx_graph graph) |
Get next free node entry in graph. More... | |
vx_status | ownGraphAddNode (vx_graph graph, vx_node node, int32_t idx) |
Add's a node to a graph. More... | |
vx_status | ownGraphRemoveNode (vx_graph graph, vx_node node) |
Remove a node from a graph. More... | |
void | ownGraphTopologicalSort (tivx_graph_sort_context *context, vx_node *nodes, uint32_t num_nodes, vx_bool *has_cycle) |
Perform topological sort of graph nodes. More... | |
vx_uint32 | ownGraphGetPipeDepth (vx_graph graph) |
Query the leaf nodes of the graph for their depth to find the total depth of the graph. More... | |
vx_bool | ownGraphCheckIsRefMatch (vx_graph graph, vx_reference ref1, vx_reference ref2) |
Abstracted check for checking if references match "vx_true_e" will be returned if references match or if references parent object matches. More... | |
void | ownGraphSetReverify (vx_graph graph) |
Mark graph to be reverified. | |
tivx_data_ref_queue | ownGraphGetParameterDataRefQueue (vx_graph graph, vx_uint32 graph_parameter_index) |
If a data ref queue is associated with 'graph_parameter_index' return it. More... | |
vx_status | ownGraphAllocAndEnqueueObjDescForPipeline (vx_graph graph) |
Alloc and enqueue graph obj desc based on graph pipeline depth. | |
vx_status | ownGraphAllocForStreaming (vx_graph graph) |
Alloc objects for graph streaming. | |
vx_status | ownGraphVerifyStreamingMode (vx_graph graph) |
verify graph schedule mode with streaming | |
vx_status | ownGraphFreeObjDesc (vx_graph graph) |
Free graph obj desc based allocated during ownGraphAllocAndEnqueueObjDescForPipeline() | |
vx_status | ownGraphFreeStreaming (vx_graph graph) |
Free graph streaming objects. | |
vx_status | ownGraphCreateQueues (vx_graph graph) |
Create queues to maintain submitted graph desc and free graph desc. | |
vx_status | ownGraphDeleteQueues (vx_graph graph) |
Delete queues created during ownGraphCreateQueues. | |
vx_status | ownGraphScheduleGraph (vx_graph graph, uint32_t num_schedule) |
Schedule a graph for execution 'num_schedule' times. | |
vx_status | ownGraphScheduleGraphWrapper (vx_graph graph) |
Wrapper for ownGraphScheduleGraph. | |
vx_bool | ownCheckGraphCompleted (vx_graph graph, uint32_t pipeline_id) |
Check if a previously scheduled graph execution is complete. More... | |
vx_bool | ownGraphDoScheduleGraphAfterEnqueue (vx_graph graph, uint32_t graph_parameter_index) |
Check if a graph should be scheduled after a graph parameter has been enqueued. More... | |
vx_status | ownUpdateGraphPerf (vx_graph graph, uint32_t pipeline_id) |
Update graph performance. | |
void | ownGraphClearState (vx_graph graph, uint32_t pipeline_id) |
Graph execution state for given pipeline ID. | |
void | ownSetGraphState (vx_graph graph, uint32_t pipeline_id, vx_enum state) |
Set graph state for a given pipeline ID. | |
vx_status | ownGraphRegisterCompletionEvent (vx_graph graph, vx_uint32 app_value) |
Register event on graph completion. | |
vx_status | ownGraphRegisterParameterConsumedEvent (vx_graph graph, uint32_t graph_parameter_index, vx_uint32 app_value) |
Register event on graph parameter consumed. | |
void | ownSendGraphCompletedEvent (vx_graph graph) |
Send graph completion event if enabled. | |
vx_status | ownGraphParameterCheckValidEnqueueRef (vx_graph graph, uint32_t graph_parameter_index, vx_reference ref) |
Checks if 'ref' is valid ref that can be enqueued. More... | |
uint32_t | ownGraphGetNumSchedule (vx_graph graph) |
Counts number of enqueued 'refs' and returns number of times graph can be scheduled successfully. More... | |
vx_status | ownGraphValidatePipelineParameters (vx_graph graph) |
Checks for invalid pipelining conditions (see: TIOVX-726) | |
void | ownGraphDetectAndSetNumBuf (vx_graph graph) |
Sets buffers automatically if not already set (see: TIOVX-903) | |
vx_status | tivxSendUserGraphEvent (vx_graph graph, vx_uint32 app_value, const void *parameter) |
Sends user event to graph event queue. | |
vx_status | tivxWaitGraphEvent (vx_graph graph, vx_event_t *event, vx_bool do_not_block) |
Waits for user event from graph event queue. | |
vx_status | tivxGraphParameterEnqueueReadyRef (vx_graph graph, vx_uint32 graph_parameter_index, vx_reference *refs, vx_uint32 num_refs, vx_uint32 flags) |
Same as vxGraphParameterEnqueueReadyRef except that it take an additional TIOVX specific flag parameter. More... | |
Implementation of Graph object.
Definition in file vx_graph.h.