TIOVX User Guide
|
Implementation of Data Reference Queue Object APIs. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_data_ref_queue_t |
Data Ref Queue internal state. More... | |
struct | tivx_data_ref_queue_create_params_t |
Parameters used to create a data ref queue. More... | |
Typedefs | |
typedef struct _tivx_data_ref_queue * | tivx_data_ref_queue |
Data Ref Queue Object. | |
Functions | |
tivx_data_ref_queue | tivxDataRefQueueCreate (vx_graph graph, const tivx_data_ref_queue_create_params_t *prms) |
Create data reference queue. | |
vx_status | ownDataRefQueueRelease (tivx_data_ref_queue *ref) |
Release data reference queue. | |
uint16_t | ownDataRefQueueGetObjDescId (tivx_data_ref_queue ref, uint32_t pipeline_id) |
return object descriptor ID of specific pipeline ID | |
vx_status | ownDataRefQueueEnqueueReadyRef (tivx_data_ref_queue data_ref_q, vx_reference ref) |
Enqueue 'ref' into 'READY' queue. More... | |
vx_status | ownDataRefQueueDequeueDoneRef (tivx_data_ref_queue data_ref_q, vx_reference *ref) |
Dequeue 'ref' from 'DONE' queue. More... | |
vx_status | ownDataRefQueueWaitDoneRef (tivx_data_ref_queue data_ref_q, vx_uint32 timeout) |
Wait for 'DONE' queue to be non-empty. More... | |
vx_status | ownDataRefQueueGetDoneQueueCount (tivx_data_ref_queue data_ref_q, vx_uint32 *count) |
Return number of elements in 'DONE' queue. | |
vx_status | ownDataRefQueueGetReadyQueueCount (tivx_data_ref_queue data_ref_q, vx_uint32 *count) |
Return number of elements in 'READY' queue. | |
vx_status | ownDataRefQueueSendRefConsumedEvent (tivx_data_ref_queue ref, uint64_t timestamp) |
Send 'ref consumed event' if event send is enabled. | |
vx_status | ownDataRefQueueLinkDelayDataRefQueues (tivx_data_ref_queue delay_data_ref_q_list[], vx_bool auto_age_delay_slot[], uint32_t delay_slots) |
Link data ref queues that participate in a delay in a circular manner. | |
Implementation of Data Reference Queue Object APIs.
Definition in file tivx_data_ref_queue.h.
vx_status ownDataRefQueueEnqueueReadyRef | ( | tivx_data_ref_queue | data_ref_q, |
vx_reference | ref | ||
) |
Enqueue 'ref' into 'READY' queue.
if queue is full, VX_FAILURE is returned.
NOTE, this is a non-blocking API.
vx_status ownDataRefQueueDequeueDoneRef | ( | tivx_data_ref_queue | data_ref_q, |
vx_reference * | ref | ||
) |
Dequeue 'ref' from 'DONE' queue.
if queue is empty VX_FAILURE is returned and 'ref' is set to NULL
NOTE, this is a non-blocking API.
vx_status ownDataRefQueueWaitDoneRef | ( | tivx_data_ref_queue | data_ref_q, |
vx_uint32 | timeout | ||
) |
Wait for 'DONE' queue to be non-empty.
if 'timeout' units of time elapses then VX_FAILURE is returned
NOTE, this is a blocking API and block for 'timeout' units of time