TIOVX User Guide
|
Graph static configuration values.
Defines | |
#define | TIVX_DEFAULT_GRAPH_TIMEOUT (TIVX_EVENT_TIMEOUT_WAIT_FOREVER) |
Default timeout value for graph level control event ACK waits. This is the default timeout value used within the following APIs. More... | |
#define | TIVX_GRAPH_PARAMETER_ENQUEUE_FLAG_PIPEUP (0x00000001u) |
Flag used with tivxGraphParameterEnqueueReadyRef to indicate that this enqueue call if for pipeup phase. More... | |
#define | TIVX_GRAPH_MAX_SUPER_NODES (8u) |
Max possible super nodes in graph. | |
Functions | |
vx_status | tivxGraphParameterEnqueueReadyRef (vx_graph graph, vx_uint32 graph_parameter_index, vx_reference *refs, vx_uint32 num_refs, vx_uint32 flags) |
Same as vxGraphParameterEnqueueReadyRef except that it take an additional TIOVX specific flag parameter. More... | |
#define TIVX_DEFAULT_GRAPH_TIMEOUT (TIVX_EVENT_TIMEOUT_WAIT_FOREVER) |
Default timeout value for graph level control event ACK waits. This is the default timeout value used within the following APIs.
Definition at line 38 of file vx_graph.h.
#define TIVX_GRAPH_PARAMETER_ENQUEUE_FLAG_PIPEUP (0x00000001u) |
Flag used with tivxGraphParameterEnqueueReadyRef to indicate that this enqueue call if for pipeup phase.
Typically used only with source nodes which have a pipeup requirement
Definition at line 49 of file vx_graph.h.
vx_status tivxGraphParameterEnqueueReadyRef | ( | vx_graph | graph, |
vx_uint32 | graph_parameter_index, | ||
vx_reference * | refs, | ||
vx_uint32 | num_refs, | ||
vx_uint32 | flags | ||
) |
Same as vxGraphParameterEnqueueReadyRef except that it take an additional TIOVX specific flag parameter.
For valid values of flag see
For more detailed description of vxGraphParameterEnqueueReadyRef see vxGraphParameterEnqueueReadyRef
[in] | graph | Graph reference |
[in] | graph_parameter_index | Graph parameter index |
[in] | refs | The array of references to enqueue into the graph parameter |
[in] | num_refs | Number of references to enqueue |
[in] | flags | Flag to control behavior of the operation |
vx_status_e
enumeration. VX_SUCCESS | No errors. |
VX_ERROR_INVALID_REFERENCE | graph is not a valid reference OR reference is not a valid reference |
VX_ERROR_INVALID_PARAMETERS | graph_parameter_index is NOT a valid graph parameter index |
VX_FAILURE | Reference could not be enqueued. |