TIOVX User Guide
|
The top level context data for the entire OpenVX instance. More...
#include <vx_context.h>
Data Fields | |
tivx_reference_t | base |
The base reference object. | |
vx_reference | reftable [TIVX_CONTEXT_MAX_REFERENCES] |
References associated with a context. | |
vx_uint32 | num_references |
The number of references in the table. | |
vx_uint32 | num_unique_kernels |
The combined number of unique kernels in the system. | |
vx_log_callback_f | log_callback |
Callback to call for logging messages from framework. | |
vx_bool | log_enabled |
The log enable toggle. | |
tivx_mutex | log_lock |
Lock to use for locking log print's. | |
tivx_mutex | lock |
Lock to use for locking context. | |
vx_bool | perf_enabled |
The performance counter enable toggle. | |
vx_border_t | imm_border |
The immediate mode border. | |
vx_enum | imm_border_policy |
The unsupported border mode policy for immediate mode functions. | |
vx_bool | is_dynamic_user_kernel_id_used [TIVX_MAX_KERNEL_ID] |
Flag indicating whether corresponding dynamic_user_kernel_id is being used. | |
vx_uint32 | num_dynamic_user_kernel_id |
Number of dynamic_user_kernel_id's being used. | |
vx_bool | is_dynamic_user_library_id_used [TIVX_MAX_LIBRARY_ID] |
Flag indicating whether corresponding dynamic_user_library_id is being used. | |
vx_uint32 | num_dynamic_user_library_id |
Number of dynamic_user_library_id's being used. | |
vx_enum | imm_target_enum |
The immediate mode enumeration. | |
vx_char | imm_target_string [TIVX_TARGET_MAX_NAME] |
The immediate mode target string. | |
tivx_user_structs_t | user_structs [TIVX_CONTEXT_MAX_USER_STRUCTS] |
The list of user defined structs. | |
vx_kernel | kerneltable [TIVX_CONTEXT_MAX_KERNELS] |
tivx_obj_desc_cmd_t * | obj_desc_cmd [TIVX_MAX_CTRL_CMD_OBJECTS] |
tivx_event | cmd_ack_event [TIVX_MAX_CTRL_CMD_OBJECTS] |
tivx_queue | free_queue |
handle to free queue holding tivx_event_queue_elem_t's NOTE: queue holds index's to event_list[] | |
uintptr_t | free_queue_memory [TIVX_MAX_CTRL_CMD_OBJECTS] |
free queue memory | |
tivx_queue | pend_queue |
handle to ready queue holding tivx_event_queue_elem_t's which are ready to be delivered to users NOTE: queue holds index's to event_list[] | |
uintptr_t | pend_queue_memory [TIVX_MAX_CTRL_CMD_OBJECTS] |
free queue memory | |
vx_bool | remove_kernel_lock |
tivx_graph_sort_context | graph_sort_context |
tivx_event_queue_t | event_queue |
The top level context data for the entire OpenVX instance.
Definition at line 75 of file vx_context.h.
vx_kernel tivx_context_t::kerneltable[TIVX_CONTEXT_MAX_KERNELS] |
Information about all kernels suported in this context
Definition at line 117 of file vx_context.h.
tivx_obj_desc_cmd_t* tivx_context_t::obj_desc_cmd[TIVX_MAX_CTRL_CMD_OBJECTS] |
Command object that is used to send control messages to different target
Definition at line 120 of file vx_context.h.
tivx_event tivx_context_t::cmd_ack_event[TIVX_MAX_CTRL_CMD_OBJECTS] |
Event used to received a command ACK
Definition at line 123 of file vx_context.h.
vx_bool tivx_context_t::remove_kernel_lock |
Flag to disallow kernel removal, used for built in kernels added during context create
Definition at line 145 of file vx_context.h.
tivx_graph_sort_context tivx_context_t::graph_sort_context |
Context used while sorting a graph
Definition at line 148 of file vx_context.h.
tivx_event_queue_t tivx_context_t::event_queue |
Event queue
Definition at line 151 of file vx_context.h.