![]() |
TIOVX User Guide
|
Internal APIs for context operations.
Data Structures | |
struct | tivx_graph_sort_context |
Context used while sorting a graph. More... | |
struct | tivx_context_t |
The top level context data for the entire OpenVX instance. More... | |
Functions | |
vx_bool | ownIsValidContext (vx_context context) |
Check if 'context' is valid. More... | |
vx_status | ownContextFlushCmdPendQueue (vx_context context) |
Flushes the command pend queue, if not empty. More... | |
vx_bool | ownAddReferenceToContext (vx_context context, vx_reference ref) |
Add reference to a context. More... | |
vx_bool | ownRemoveReferenceFromContext (vx_context context, vx_reference ref) |
Remove reference from a context. More... | |
vx_status | ownAddKernelToContext (vx_context context, vx_kernel kernel) |
Add's unique kernel to context. More... | |
vx_status | ownRemoveKernelFromContext (vx_context context, vx_kernel kernel) |
Remove unique kernel from context. More... | |
vx_status | ownIsKernelInContext (vx_context context, vx_enum enumeration, const vx_char string[VX_MAX_KERNEL_NAME], vx_bool *is_found) |
Check if kernel exists inside the context. | |
vx_status | ownContextSendCmd (vx_context context, uint32_t target_id, uint32_t cmd, uint32_t num_obj_desc, const uint16_t *obj_desc_id, uint32_t timeout) |
Send a command to specified target with object descriptor ID's as parameters. More... | |
vx_status | ownContextSendControlCmd (vx_context context, uint16_t node_obj_desc, uint32_t target_id, uint32_t replicated_node_idx, uint32_t node_cmd_id, const uint16_t obj_desc_id[], uint32_t num_obj_desc, uint32_t timeout) |
Send a control command to specified target with object descriptor ID's as parameters. More... | |
vx_bool | ownContextGetKernelRemoveLock (vx_context context) |
Get value of kernel remove lock flag. More... | |
void | ownContextSetKernelRemoveLock (vx_context context, vx_bool do_lock) |
Set value of kernel remove lock flag. More... | |
vx_status | ownContextLock (vx_context context) |
Lock context. More... | |
vx_status | ownContextUnlock (vx_context context) |
Lock context. More... | |
vx_context | ownGetContext (void) |
Returns the vx_context object currently being used. More... | |
vx_bool ownIsValidContext | ( | vx_context | context | ) |
Check if 'context' is valid.
[in] | context | The reference to context |
vx_status_e
enumeration. VX_SUCCESS | No errors. |
vx_status ownContextFlushCmdPendQueue | ( | vx_context | context | ) |
Flushes the command pend queue, if not empty.
[in] | context | The reference to context |
vx_status_e
enumeration. VX_SUCCESS | No errors. |
vx_bool ownAddReferenceToContext | ( | vx_context | context, |
vx_reference | ref | ||
) |
Add reference to a context.
[in] | context | The overall context. |
[in] | ref | The reference to add. |
vx_bool ownRemoveReferenceFromContext | ( | vx_context | context, |
vx_reference | ref | ||
) |
Remove reference from a context.
[in] | context | The overall context. |
[in] | ref | The reference to remove. |
vx_status ownAddKernelToContext | ( | vx_context | context, |
vx_kernel | kernel | ||
) |
Add's unique kernel to context.
Increment internal reference count of the kernel
vx_status ownRemoveKernelFromContext | ( | vx_context | context, |
vx_kernel | kernel | ||
) |
Remove unique kernel from context.
Decrement internal reference count of the kernel
vx_status ownContextSendCmd | ( | vx_context | context, |
uint32_t | target_id, | ||
uint32_t | cmd, | ||
uint32_t | num_obj_desc, | ||
const uint16_t * | obj_desc_id, | ||
uint32_t | timeout | ||
) |
Send a command to specified target with object descriptor ID's as parameters.
This API waits until ACK for the command is received
context | [in] context to use when sending the command |
target_id | [in] ID of Target to whom the command is being sent |
cmd | [in] command to send |
num_obj_desc | [in] number of object descriptors to send |
obj_desc_id | [in] List of object descriptor to send |
timeout | [in] Timeout in units of msecs, use TIVX_EVENT_TIMEOUT_WAIT_FOREVER to wait forever |
vx_status ownContextSendControlCmd | ( | vx_context | context, |
uint16_t | node_obj_desc, | ||
uint32_t | target_id, | ||
uint32_t | replicated_node_idx, | ||
uint32_t | node_cmd_id, | ||
const uint16_t | obj_desc_id[], | ||
uint32_t | num_obj_desc, | ||
uint32_t | timeout | ||
) |
Send a control command to specified target with object descriptor ID's as parameters.
This API waits for 'timeout' msecs, until ACK for the command is received
context | [in] context to use when sending the command |
node_obj_desc | [in] ID of node object descriptor to which command is being sent |
target_id | [in] ID of Target to whom the command is being sent |
replicated_node_idx | [in] If the node is replicated, index of the replica to send the command to |
node_cmd_id | [in] ID of the command to send to the node |
obj_desc_id[] | [in] Array of IDs of object descriptor |
num_obj_desc | [in] Number of object descriptors in obj_desc_id[] array |
timeout | [in] Timeout in units of msecs, use TIVX_EVENT_TIMEOUT_WAIT_FOREVER to wait forever |
vx_bool ownContextGetKernelRemoveLock | ( | vx_context | context | ) |
Get value of kernel remove lock flag.
context | [in] context |
void ownContextSetKernelRemoveLock | ( | vx_context | context, |
vx_bool | do_lock | ||
) |
Set value of kernel remove lock flag.
context | [in] context |
do_lock | [in] kernel remove lock value to set |
vx_status ownContextLock | ( | vx_context | context | ) |
Lock context.
context | [in] context |
vx_status ownContextUnlock | ( | vx_context | context | ) |
Lock context.
context | [in] context |
vx_context ownGetContext | ( | void | ) |
Returns the vx_context object currently being used.
This API returns the context being used. If the context has not yet been created using vxCreateContext, then it returns NULL. This API does not include reference counting like in the vxCreateContext.
vx_context
object being used.