3.7. RTI Safety Example¶
3.7.1. Introduction¶
This example displays setting up RTI to
Setup of Windowed Watchdog Timer (WWDT)
Handling WWDT failure interrupts received on the ESM module in the MCU domain R5F
3.7.2. Use Cases¶
Use Case
Failure n
RTI Inst
ESM
Window
Input Trigger
Expected Event
UC-1
Permanent Failure (100% Window)
RTI0
MCU_ESM0
100%
Stop servicing completely
Window End
UC-2
Permanent Failure (50% Window)
RTI0
MCU_ESM0
50%
Stop servicing completely
Window End
UC-3
Latency / Propagation timing error (early) (50% window)
RTI0
MCU_ESM0
50%
Service before window opens again after previous feeding
Window Start
UC-4
Latency / Propagation timing error (late) (50% window)
RTI0
MCU_ESM0
50%
Service after full window has passed since previous feeding
Window End, then Window Start
3.7.3. Example Details¶
The example should be loaded to the hardware using the Secondary Boot Loader (SBL) from the SDK.
Example Name |
Location |
Build Command |
|---|---|---|
rti_app_uc1 |
[sdl_install_dir]/examples/rti/UC1/ |
make rti_app_uc1 PROFILE=release |
rti_app_uc2 |
[sdl_install_dir]/examples/rti/UC2/ |
make rti_app_uc2 PROFILE=release |
rti_app_uc3 |
[sdl_install_dir]/examples/rti/UC3/ |
make rti_app_uc3 PROFILE=release |
rti_app_uc4 |
[sdl_install_dir]/examples/rti/UC4 |
make rti_app_uc4 PROFILE=release |
3.7.4. Expected Output¶
rti_app_uc1:
RTI Example Test Application
RTI_Test_init: Init MCU ESM complete
RTI Example code UC-1 started
DWWD configured to 100 percent window size
DWWD is configured for 10000 ms time-out
RTI DWWD proper servicing test running.
Please wait for max 10000 ms.
RTI DWWD proper servicing test successful.
RTI permanent failure test running.
DWWD will generate interrupt after 10 seconds
Wait for 10 sec for interrupt to be generated by DWWD.
Interrupt is generated to ESM
ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x2, index 0x14, intSrc 0x54
Take action
RTI Window End time violation test successful.
Test Name: RTI EXAMPLE TEST PASSED
All tests have passed.
rti_app_uc2:
RTI Example Test Application
RTI_Test_init: Init MCU ESM complete
RTI Example code UC-2 started
DWWD configured to 50 percent window size
DWWD is configured for 10000 ms time-out
RTI DWWD proper servicing test running.
Please wait for max 10000 ms.
RTI DWWD proper servicing test successful.
RTI permanent failure test running.
DWWD will generate interrupt after 10 seconds
Wait for 10 sec for interrupt to be generated by DWWD.
Interrupt is generated to ESM
ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x2, index 0x14, intSrc 0x54
Take action
RTI Window End time violation test successful.
Test Name: RTI EXAMPLE TEST PASSED
All tests have passed.
rti_app_uc3:
RTI Example Test Application
RTI_Test_init: Init MCU ESM complete
RTI Example code UC-3 started
DWWD configured to 50 percent window size
DWWD is configured for 10000 ms time-out
RTI DWWD Early Trigger violation test running.
Servicing before the window open.
Interrupt is generated to ESM
ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x2, index 0x14, intSrc 0x54
Take action
RTI DWWD Early Trigger violation test successful.
Test Name: RTI EXAMPLE TEST PASSED
All tests have passed.
rti_app_uc4:
RTI Example Test Application
RTI_Test_init: Init MCU ESM complete
RTI Example code UC-4 started
DWWD configured to 50 percent window size
DWWD is configured for 10000 ms time-out
DWWD will generate interrupt after 10 seconds
Waiting for window to expire
Wait for 10 sec for interrupt to be generated by DWWD.
Interrupt is generated to ESM
ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x2, index 0x14, intSrc 0x54
Take action
RTI Late trigger servicing test running.
Re-Opening the window to service after previous feed
RTI Late trigger servicing test successful.
Test Name: RTI EXAMPLE TEST PASSED
All tests have passed.