![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 141 of file DSPLIB_bexp_priv.h.
Data Fields | |
| pFxnDSPLIB_bexp_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_bexp_exec_cn and DSPLIB_bexp_exec_ci. More... | |
| uint32_t | blockSize |
| Size of input buffer for different batches DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec More... | |
| bool | isSEReadEnabled |
| Flag indicating if SE reads are enabled, set by DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec More... | |
| uint32_t | mainLoopCount |
| Number of times to loop over data with isSEReadEnabled == true will be ceil_division(number of native vectors, 2) isSEReadEnabled == false will be number of native vectors set by DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec More... | |
| uint32_t | se1StartAddressByteOffset |
| The offset in bytes of SE1 start address with respect to start address of the input data. Set by DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec More... | |
| uint8_t | bufPblock [DSPLIB_BEXP_IXX_IXX_OXX_PBLOCK_SIZE] |
| pFxnDSPLIB_bexp_exec DSPLIB_bexp_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_bexp_exec_cn and DSPLIB_bexp_exec_ci.
Definition at line 145 of file DSPLIB_bexp_priv.h.
| uint32_t DSPLIB_bexp_PrivArgs::blockSize |
Size of input buffer for different batches DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec
Definition at line 149 of file DSPLIB_bexp_priv.h.
| bool DSPLIB_bexp_PrivArgs::isSEReadEnabled |
Flag indicating if SE reads are enabled, set by DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec
Definition at line 154 of file DSPLIB_bexp_priv.h.
| uint32_t DSPLIB_bexp_PrivArgs::mainLoopCount |
Number of times to loop over data with isSEReadEnabled == true will be ceil_division(number of native vectors, 2) isSEReadEnabled == false will be number of native vectors set by DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec
Definition at line 161 of file DSPLIB_bexp_priv.h.
| uint32_t DSPLIB_bexp_PrivArgs::se1StartAddressByteOffset |
The offset in bytes of SE1 start address with respect to start address of the input data. Set by DSPLIB_bexp_init that will be retrieved and used by DSPLIB_bexp_exec
Definition at line 167 of file DSPLIB_bexp_priv.h.
| uint8_t DSPLIB_bexp_PrivArgs::bufPblock[DSPLIB_BEXP_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 169 of file DSPLIB_bexp_priv.h.