DSPLIB User Guide
DSPLIB_bexp_priv.h File Reference

Introduction

Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_bexp.

Definition in file DSPLIB_bexp_priv.h.

Go to the source code of this file.

Data Structures

struct  DSPLIB_bexp_PrivArgs
 Structure that is reserved for internal use by the kernel. More...
 

Macros

#define DSPLIB_BEXP_IXX_IXX_OXX_MAX_BITS_PER_ELEMENT   (70)
 Macro to define the maximum number of bits in an element @ref DSPLIB_bexp_exec_ci. More...
 
#define DSPLIB_BEXP_IXX_IXX_OXX_MIN_VECS_TO_ENABLE_SE_READS   (4)
 Macro to define the minimum number of vector lengths that the input data should occupy before SE is used for data reads @ref DSPLIB_bexp_exec_ci. More...
 
#define DSPLIB_BEXP_IXX_IXX_OXX_PBLOCK_SIZE   (2 * SE_PARAM_SIZE + 512)
 Macro to print the debug message. More...
 

Typedefs

typedef DSPLIB_STATUS(* pFxnDSPLIB_bexp_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This is a function pointer type that conforms to the declaration of DSPLIB_bexp_exec_ci and DSPLIB_bexp_exec_cn. More...
 

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_bexp_InitArgs *pKerInitArgs)
 This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_exec. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_exec. More...
 
DSPLIB_STATUS DSPLIB_bexp_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut)
 This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_init. More...
 

Macro Definition Documentation

◆ DSPLIB_BEXP_IXX_IXX_OXX_MAX_BITS_PER_ELEMENT

#define DSPLIB_BEXP_IXX_IXX_OXX_MAX_BITS_PER_ELEMENT   (70)

Macro to define the maximum number of bits in an element @ref DSPLIB_bexp_exec_ci.

Definition at line 39 of file DSPLIB_bexp_priv.h.

◆ DSPLIB_BEXP_IXX_IXX_OXX_MIN_VECS_TO_ENABLE_SE_READS

#define DSPLIB_BEXP_IXX_IXX_OXX_MIN_VECS_TO_ENABLE_SE_READS   (4)

Macro to define the minimum number of vector lengths that the input data should occupy before SE is used for data reads @ref DSPLIB_bexp_exec_ci.

Definition at line 48 of file DSPLIB_bexp_priv.h.

◆ DSPLIB_BEXP_IXX_IXX_OXX_PBLOCK_SIZE

#define DSPLIB_BEXP_IXX_IXX_OXX_PBLOCK_SIZE   (2 * SE_PARAM_SIZE + 512)

Macro to print the debug message.

Definition at line 54 of file DSPLIB_bexp_priv.h.

Typedef Documentation

◆ pFxnDSPLIB_bexp_exec

typedef DSPLIB_STATUS(* pFxnDSPLIB_bexp_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)

This is a function pointer type that conforms to the declaration of DSPLIB_bexp_exec_ci and DSPLIB_bexp_exec_cn.

Definition at line 61 of file DSPLIB_bexp_priv.h.

Function Documentation

◆ DSPLIB_bexp_init_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_init_ci ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_bexp_InitArgs pKerInitArgs 
)

This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_init.

This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_bexp_exec_ci would be called later independently by the application. When DSPLIB_bexp_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_bexp_exec_ci does not lose cycles to determine the hardware configuration.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Init function of the bexp kernel to setup the SE

Definition at line 62 of file DSPLIB_bexp_ci.cpp.

◆ DSPLIB_bexp_exec_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_exec_ci ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_exec.

The function uses C7x DSP to perform the block exponent. The input data is read as blocks of vectors using the streaming engine. A vertical OR operation is performed on the blocks of vectors that are read using the streaming engine. Finally, once the entire data is read and the final OR result is computed, a horizontal OR operation is performed to get the final mask value. The number of leading zeros or redundant sign bits are computed as the exponent.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned

◆ DSPLIB_bexp_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_bexp_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_exec.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

C Natural implementation of the bexp kernels. Handles unsigned and signed data types internally

Definition at line 36 of file DSPLIB_bexp_cn.cpp.

◆ DSPLIB_bexp_init_cn()

DSPLIB_STATUS DSPLIB_bexp_init_cn ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams2D_t bufParamsIn,
DSPLIB_bufParams2D_t bufParamsOut 
)

This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_bexp_init.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.