![]() |
DSPLIB User Guide
|
The bexp kernel, performs a determination of the block exponent of the vector of elements and returns the maximum exponent.
Data Structures | |
| struct | DSPLIB_bexp_InitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_bexp_getHandleSize (DSPLIB_bexp_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_bexp_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_bexp_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_bexp_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources, streaming engine in this case. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_bexp_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_bexp_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_bexp_init function. This function is called with the same parameters as the DSPLIB_bexp_init, and this function must be called before the DSPLIB_bexp_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_bexp_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut) |
| This function checks the validity of the parameters passed to DSPLIB_bexp_exec function. This function is called with the same parameters as the DSPLIB_bexp_exec, and this function must be called before the DSPLIB_bexp_exec is called. More... | |
| DSPLIB_STATUS | DSPLIB_bexp_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main kernel compute function. More... | |
| int32_t DSPLIB_bexp_getHandleSize | ( | DSPLIB_bexp_InitArgs * | pKerInitArgs | ) |
This is a query function to calculate the size of internal handle.
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
Definition at line 29 of file DSPLIB_bexp.cpp.
| DSPLIB_STATUS DSPLIB_bexp_init | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_bexp_InitArgs * | pKerInitArgs | ||
| ) |
This function should be called before the DSPLIB_bexp_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources, streaming engine in this case. The results of these operations are stored in the handle.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 86 of file DSPLIB_bexp.cpp.
| DSPLIB_STATUS DSPLIB_bexp_init_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_bexp_InitArgs * | pKerInitArgs | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_bexp_init function. This function is called with the same parameters as the DSPLIB_bexp_init, and this function must be called before the DSPLIB_bexp_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 35 of file DSPLIB_bexp.cpp.
| DSPLIB_STATUS DSPLIB_bexp_exec_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const void *restrict | pIn, | ||
| const void *restrict | pOut | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_bexp_exec function. This function is called with the same parameters as the DSPLIB_bexp_exec, and this function must be called before the DSPLIB_bexp_exec is called.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to the structure input buffer 1 |
| [out] | pout | : Pointer to the output buffer |
Definition at line 70 of file DSPLIB_bexp.cpp.
| DSPLIB_STATUS DSPLIB_bexp_exec | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main kernel compute function.
Please refer to details under DSPLIB_bexp_exec
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 170 of file DSPLIB_bexp.cpp.