PDK API Guide for J721E
|
Cycle profiler module to measure CPU cycles for the RTOS Porting Interface.
============================================================================
Go to the source code of this file.
Functions | |
void | CycleprofilerP_init (void) |
Function to initialize cycle profiler. More... | |
uint32_t | CycleprofilerP_getTimeStamp (void) |
Function to get current timestamp. More... | |
void | CycleprofilerP_refreshCounter () |
Checks PMU timer overflow and increments the higher 32 bits. More... | |