![]() |
PDK API Guide for J721E
|
PMIC Driver Common API/interface file.
Go to the source code of this file.
Data Structures | |
struct | Pmic_RecovCntCfg_t |
PMIC Recovery Counter Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIS and output param for Get APIs. More... | |
struct | Pmic_CommonCtrlCfg_t |
PMIC common control param configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_MiscCtrlCfg_t |
PMIC Miscellaneous control param Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_BatteryCtrlCfg_t |
PMIC Backup Battery control param Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_CommonCtrlStat_t |
PMIC common control param status Note: validParams is input param for all Get APIs. other params except validParams is output param for Get APIs. More... | |
struct | Pmic_DeviceInfo_t |
PMIC Device Information. More... | |
Macros | |
#define | DRV_INIT_SUCCESS (0xABCD0000U) |
PMIC driver Core Handle INIT status Magic Number. Used to validate Handle to avoid corrupted PmicHandle usage. on Success: (DRV_INIT_SUCCESS | Pmic_InstType_t) More... | |
#define | PMIC_SILICON_REV_ID_PG_2_0 (0x08U) |
Silicon Revision Id - PG 2.0 for TPS6594x Leo and LP8764x Hera. More... | |
#define | PMIC_SILICON_REV_ID_PG_1_0 (0x0U) |
Silicon Revision Id - PG 1.0 for TPS6594x Leo and LP8764x Hera. More... | |
PMIC Recovery Counter Configuration Type | |
#define | PMIC_CFG_RECOV_CNT_THR_VAL_VALID (0U) |
validParams value used to set/get Recovery Counter Threshold Value More... | |
#define | PMIC_CFG_RECOV_CNT_CLR_CNT_VALID (1U) |
validParams value used to Clear/get Recovery Counter Value More... | |
PMIC Recovery Count Configuration Structure Param Bit shift values | |
Application can use below shifted values to set the validParams struct members defined in Pmic_RecovCntCfg_t structure | |
#define | PMIC_CFG_RECOV_CNT_THR_VAL_VALID_SHIFT (1U << PMIC_CFG_RECOV_CNT_THR_VAL_VALID) |
#define | PMIC_CFG_RECOV_CNT_CLR_CNT_VALID_SHIFT (1U << PMIC_CFG_RECOV_CNT_CLR_CNT_VALID) |
PMIC Scratchpad register selection | |
#define | PMIC_SCRATCH_PAD_REG_1 (0x0U) |
#define | PMIC_SCRATCH_PAD_REG_2 (0x1U) |
#define | PMIC_SCRATCH_PAD_REG_3 (0x2U) |
#define | PMIC_SCRATCH_PAD_REG_4 (0x3U) |
PMIC User Spare register selection | |
#define | PMIC_USER_SPARE_REG_1 (0x0U) |
#define | PMIC_USER_SPARE_REG_2 (0x1U) |
#define | PMIC_USER_SPARE_REG_3 (0x2U) |
#define | PMIC_USER_SPARE_REG_4 (0x3U) |
PMIC User Spare register Value | |
#define | PMIC_USER_SPARE_REG_VAL_0 (0x0U) |
#define | PMIC_USER_SPARE_REG_VAL_1 (0x1U) |
PMIC Common control param status Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_CommonCtrlStat_t structure | |
#define | PMIC_CFG_BB_EOC_INDICATION_STAT_VALID (0U) |
validParams value used to get Backup Battery End of charge Indication Status More... | |
#define | PMIC_CFG_REGISTER_LOCK_STAT_VALID (1U) |
validParams value used to get Register lock status More... | |
#define | PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID (2U) |
validParams value used to get External clock validity status More... | |
#define | PMIC_CFG_STARTUP_PIN_STAT_VALID (3U) |
validParams value used to get Startup(nPWRON/Enable) pin status More... | |
#define | PMIC_CFG_EN_DRV_PIN_STAT_VALID (4U) |
validParams value used to get EN_DRV Pin status More... | |
#define | PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID (5U) |
validParams value used to get nRSTOUT_SOC Pin status More... | |
#define | PMIC_CFG_NRSTOUT_PIN_STAT_VALID (6U) |
validParams value used to get nRSTOUT Pin status More... | |
#define | PMIC_CFG_NINT_PIN_STAT_VALID (7U) |
validParams value used to get nINT Pin status More... | |
#define | PMIC_CFG_SPMI_LPM_STAT_VALID (8U) |
validParams value used to get SPMI Low Power Mode status More... | |
#define | PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID (9U) |
validParams value used to get status of ENABLE_DRV Configuration by I2C/SPI More... | |
PMIC Common Control param status valid param bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_CommonCtrlStat_t structure | |
#define | PMIC_CFG_BB_EOC_INDICATION_STAT_VALID_SHIFT (1U << PMIC_CFG_BB_EOC_INDICATION_STAT_VALID) |
#define | PMIC_CFG_REGISTER_LOCK_STAT_VALID_SHIFT (1U << PMIC_CFG_REGISTER_LOCK_STAT_VALID) |
#define | PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID_SHIFT (1U << PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID) |
#define | PMIC_CFG_STARTUP_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_STARTUP_PIN_STAT_VALID) |
#define | PMIC_CFG_EN_DRV_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_EN_DRV_PIN_STAT_VALID) |
#define | PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID) |
#define | PMIC_CFG_NRSTOUT_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_PIN_STAT_VALID) |
#define | PMIC_CFG_NINT_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NINT_PIN_STAT_VALID) |
#define | PMIC_CFG_SPMI_LPM_STAT_VALID_SHIFT (1U << PMIC_CFG_SPMI_LPM_STAT_VALID) |
#define | PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID_SHIFT (1U << PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID) |
PMIC signal level of the STARTUP(NPWRON/ENABLE)/ NINT / NRSTOUT_SOC/ | |
#define | PMIC_PIN_SIGNAL_LEVEL_LOW (0U) |
#define | PMIC_PIN_SIGNAL_LEVEL_HIGH (1U) |
PMIC Pin Type Selection as NRSTOUT_SOC/ NRSTOUT/ EN_DRV | |
#define | PMIC_PIN_TYPE_EN_DRV (0U) |
#define | PMIC_PIN_TYPE_NRSTOUT_SOC (1U) |
#define | PMIC_PIN_TYPE_NRSTOUT (2U) |
PMIC ENABLE_DRV I2C/SPI configuration status | |
#define | PMIC_ENABLE_DRV_I2C_SPI_CONFIG_ENABLE (0U) |
#define | PMIC_ENABLE_DRV_I2C_SPI_CONFIG_DISABLE (1U) |
PMIC Register Lock Configuration | |
#define | PMIC_REGISTER_UNLOCK (0x9BU) |
Unlock PMIC Registers. More... | |
#define | PMIC_REGISTER_LOCK (0x10U) |
Lock PMIC Registers - Write any value other than 0x9B. Here 0x10 is used. More... | |
PMIC Register Lock Status | |
#define | PMIC_REGISTER_STATUS_UNLOCK (0x0U) |
#define | PMIC_REGISTER_STATUS_LOCK (0x1U) |
PMIC Spread Spectrum Configuration | |
#define | PMIC_SPREAD_SPECTRUM_CFG_DISABLE 0U |
Disable Spread Spectrum Configuration. More... | |
#define | PMIC_SPREAD_SPECTRUM_CFG_ENABLE 1U |
Enable Spread Spectrum Configuration. More... | |
PMIC Spread Spectrum Modulation Depth Sel | |
#define | PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_NONE (0U) |
No Modulation. More... | |
#define | PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_6_3_PERCENT (1U) |
Modulation Depth as +/- 6.3%. More... | |
#define | PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_8_4_PERCENT (2U) |
Modulation Depth as +/- 8.4%. More... | |
PMIC SPMI LPM Mode Control Status | |
#define | PMIC_SPMI_LPM_MODE_CTRL_CFG_DISABLED (0U) |
SPMI LPM Mode Control Configuration is Disabled. More... | |
#define | PMIC_SPMI_LPM_MODE_CTRL_CFG_ENABLED (1U) |
SPMI LPM Mode Control Configuration is Enabled. More... | |
PMIC Internal Clock Monitoring Configuration | |
#define | PMIC_INTERNAL_CLK_MONITORING_CFG_DISABLE (0U) |
Disable Internal Clock Monitoring. More... | |
#define | PMIC_INTERNAL_CLK_MONITORING_CFG_ENABLE (1U) |
Enable Internal Clock Monitoring. More... | |
PMIC SYNCCLKOUT Frequency selection | |
#define | PMIC_SYNCCLKOUT_DISABLE (0U) |
DISABLE SYNCCLKOUT. More... | |
#define | PMIC_SYNCCLKOUT_1_1_MHZ (1U) |
SYNCCLKOUT Frequency as 1.1 MHz. More... | |
#define | PMIC_SYNCCLKOUT_2_2_MHZ (2U) |
SYNCCLKOUT Frequency as 2.2 MHz. More... | |
#define | PMIC_SYNCCLKOUT_4_4_MHZ (3U) |
SYNCCLKOUT Frequency as 4.4 MHz. More... | |
PMIC External Clock selection | |
#define | PMIC_INTERNAL_RC_OSC (0U) |
Forced to Internal RC Oscillator. More... | |
#define | PMIC_AUTOMATIC_EXT_CLK (1U) |
Selects External clock when Available. More... | |
PMIC External Clock Validity Status | |
#define | PMIC_EXT_CLK_STATUS_VALID (0U) |
#define | PMIC_EXT_CLK_STATUS_INVALID (1U) |
PMIC CRC Status for I2C1/I2C2/SPI | |
#define | PMIC_CRC_STATUS_DISABLED (0U) |
CRC is disabled. More... | |
#define | PMIC_CRC_STATUS_ENABLED (1U) |
CRC is enabled. More... | |
PMIC Common Control Configuration Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_CommonCtrlCfg_t structure | |
#define | PMIC_CFG_SPREAD_SPECTRUM_EN_VALID (0U) |
validParams value used to set/get Spread Spectrum Enable/Disable More... | |
#define | PMIC_CFG_ENABLE_DRV_VALID (1U) |
validParams value used to set/get ENABLE_DRV pin configuration More... | |
#define | PMIC_CFG_REG_LOCK_VALID (2U) |
validParams value used to set/get Register Lock configuration More... | |
#define | PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID (3U) |
validParams value used to set/get Spread Spectrum modulation Depth Value More... | |
#define | PMIC_CFG_EEPROM_DEFAULT_VALID (4U) |
validParams value used to set/get to Enable/Disable load from EEPROM defaults on RTC Domain(TPS6594X Leo)/ conf(LP8764x Hera) registers More... | |
#define | PMIC_CFG_SKIP_EEPROM_LOAD_VALID (5U) |
validParams value used to set/get to Enable/Disable to skip EEPROM defaults load on conf and Other registers Valid only for LP8764x Hera More... | |
PMIC Common Control Configuration valid param bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_CommonCtrlCfg_t structure | |
#define | PMIC_CFG_SPREAD_SPECTRUM_EN_VALID_SHIFT (1U << PMIC_CFG_SPREAD_SPECTRUM_EN_VALID) |
#define | PMIC_CFG_ENABLE_DRV_VALID_SHIFT (1U << PMIC_CFG_ENABLE_DRV_VALID) |
#define | PMIC_CFG_REG_LOCK_VALID_SHIFT (1U << PMIC_CFG_REG_LOCK_VALID) |
#define | PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID_SHIFT (1U << PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID) |
#define | PMIC_CFG_EEPROM_DEFAULT_VALID_SHIFT (1U << PMIC_CFG_EEPROM_DEFAULT_VALID) |
#define | PMIC_CFG_SKIP_EEPROM_LOAD_VALID_SHIFT (1U << PMIC_CFG_SKIP_EEPROM_LOAD_VALID) |
PMIC Miscellaneous Control Configuration Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_MiscCtrlCfg_t structure | |
#define | PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Band gap Voltage to AMUX OUT/REF OUT Pin More... | |
#define | PMIC_CFG_CLK_MON_EN_VALID (1U) |
validParams value used to set/get to Enable or Disable internal Clock Monitoring More... | |
#define | PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID (2U) |
validParams value used to set/get to Select SYNCCLKOUT Frequency More... | |
#define | PMIC_CFG_EXT_CLK_SEL_VALID (3U) |
validParams value used to set/get External clock Selection More... | |
#define | PMIC_CFG_SYNC_CLK_IN_FREQ_VALID (4U) |
validParams value used to set/get to Select External clock Frequency More... | |
#define | PMIC_CFG_NRSTOUT_SOC_VALID (5U) |
validParams value used to set/get to NRSTOUT_SOC Signal More... | |
#define | PMIC_CFG_NRSTOUT_VALID (6U) |
validParams value used to set/get NRSTOUT Signal More... | |
PMIC Miscellaneous Control Configuration valid param bit shift | |
Application can use below shifted values to set the validParam member defined in Pmic_MiscCtrlCfg_t structure | |
#define | PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID_SHIFT (1U << PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID) |
#define | PMIC_CFG_CLK_MON_EN_VALID_SHIFT (1U << PMIC_CFG_CLK_MON_EN_VALID) |
#define | PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID_SHIFT (1U << PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID) |
#define | PMIC_CFG_EXT_CLK_SEL_VALID_SHIFT (1U << PMIC_CFG_EXT_CLK_SEL_VALID) |
#define | PMIC_CFG_SYNC_CLK_IN_FREQ_VALID_SHIFT (1U << PMIC_CFG_SYNC_CLK_IN_FREQ_VALID) |
#define | PMIC_CFG_NRSTOUT_SOC_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_SOC_VALID) |
#define | PMIC_CFG_NRSTOUT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_VALID) |
PMIC Backup Battery Control Configuration Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_BatteryCtrlCfg_t structure | |
#define | PMIC_CFG_CHARGING_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Backup Battery Charging More... | |
#define | PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID (1U) |
validParams value used to set/get to Backup Battery configuration for End of charge Voltage More... | |
#define | PMIC_CFG_CHARGE_CURRENT_VALID (2U) |
validParams value used to set/get to Backup Battery charging current value More... | |
PMIC Backup Battery Control Configuration valid param bit shift | |
Application can use below shifted values to set the validParam member defined in Pmic_BatteryCtrlCfg_t structure | |
#define | PMIC_CFG_CHARGING_EN_VALID_SHIFT (1U << PMIC_CFG_CHARGING_EN_VALID) |
#define | PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID_SHIFT (1U << PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID) |
#define | PMIC_CFG_CHARGE_CURRENT_VALID_SHIFT (1U << PMIC_CFG_CHARGE_CURRENT_VALID) |
Functions | |
int32_t | Pmic_setRecoveryCntCfg (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_RecovCntCfg_t recovCntCfg) |
API to Set Recovery Counter Configuration. More... | |
int32_t | Pmic_getRecoveryCntCfg (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_RecovCntCfg_t *pRecovCntCfg) |
API to Get Recovery Counter Configuration. More... | |
int32_t | Pmic_getRecoveryCnt (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pRecovCntVal) |
API to Read Recovery Count Value. More... | |
int32_t | Pmic_setScratchPadValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t scratchPadRegNum, const uint8_t data) |
API to set/write value in/to scratchpad register. More... | |
int32_t | Pmic_getScratchPadValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t scratchPadRegNum, uint8_t *pData) |
API to get/read data from scratchpad register. More... | |
int32_t | Pmic_setUserSpareValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t userSpareRegNum, const uint8_t data) |
API to set/write value in/to User Spare register. More... | |
int32_t | Pmic_getUserSpareValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t userSpareRegNum, uint8_t *pData) |
API to get/read data from User Spare register. More... | |
int32_t | Pmic_setCommonCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_CommonCtrlCfg_t commonCtrlCfg) |
API to set PMIC common control parameter configuration. More... | |
int32_t | Pmic_getCommonCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_CommonCtrlCfg_t *pCommonCtrlCfg) |
API to get PMIC common control parameter configuration. More... | |
int32_t | Pmic_setMiscCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_MiscCtrlCfg_t miscCtrlCfg) |
API to set PMIC Miscellaneous control parameter configuration. More... | |
int32_t | Pmic_getMiscCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_MiscCtrlCfg_t *pMiscCtrlCfg) |
API to get PMIC Miscellaneous control parameter configuration. More... | |
int32_t | Pmic_setBatteryCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_BatteryCtrlCfg_t batteryCtrlCfg) |
API to set PMIC Battery Backup control parameter configuration. More... | |
int32_t | Pmic_getBatteryCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_BatteryCtrlCfg_t *pBatteryCtrlCfg) |
API to get PMIC Battery Backup control parameter configuration. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
int32_t | Pmic_getPinValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pinType, uint8_t *pPinValue) |
API to get PMIC GPIO NRSTOUT_SOC/ NRSTOUT/ EN_DRV Pin. More... | |
int32_t | Pmic_getCommonCtrlStat (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_CommonCtrlStat_t *pCommonCtrlStat) |
API to get PMIC common control parameter status. More... | |
int32_t | Pmic_getI2CSpeed (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pI2C1Speed, uint8_t *pI2C2Speed) |
API to get configured value for I2C1 or I2C2 Speed based on commMode. More... | |
int32_t | Pmic_enableCRC (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to Enable CRC. More... | |
int32_t | Pmic_getCrcStatus (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pI2c1SpiCrcStatus, uint8_t *pI2c2CrcStatus) |
API to get CRC Status. More... | |
int32_t | Pmic_getDeviceInfo (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_DeviceInfo_t *pDeviceInfo) |
API to get PMIC Device Information. More... | |
int32_t | Pmic_setI2CSpeedCfg (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to set I2C1 or I2C2 Speed based on commMode. More... | |