PDK API Guide for J721E
|
Structure containing display driver create arguments, used when calling Fvid2_create(). Application shall maintain same create time configurations between multiple driver handles for same WB pipe-line.
Data Fields | |
uint32_t | numPipe |
uint32_t | pipeId [DSSM2M_NUM_PIPELINE_TO_USE_IN_M2M_MODE] |
uint32_t | overlayId |
uint32_t Dss_WbCreateParams::numPipe |
Number of Display pipe-lines used for given M2M/WB pipeline. This should be set to '1' (as done in Dss_m2mCreateParamsInit())
uint32_t Dss_WbCreateParams::pipeId[DSSM2M_NUM_PIPELINE_TO_USE_IN_M2M_MODE] |
ID DSS pipeline to use. Application shall only set pipe IDs which are used. See CSL_DssVidPipeId for details
uint32_t Dss_WbCreateParams::overlayId |
ID DSS overlay to use. See CSL_DssOverlayId for details