This is DSS Display Write-back driver documentation
|
file | dss_m2m.h |
| DSS Display Write-back Driver interface file.
|
|
|
struct | Dss_WbPipeCfgParams |
| Structure containing video write-back pipe configuration. More...
|
|
struct | Dss_WbPipeMflagParams |
| Structure containing Video write-back Pipe Mflag Information. This structure is used as an argument to IOCTL_DSS_M2M_SET_WB_PIPE_MFLAG_PARAMS. More...
|
|
struct | Dss_WbStatus |
| Structure containing current status of the display M2M driver. This structure is used as an argument to IOCTL_DSS_M2M_GET_CURRENT_STATUS. More...
|
|
struct | Dss_WbCreateParams |
| Structure containing display driver create arguments, used when calling Fvid2_create(). Application shall maintain same create time configurations between multiple driver handles for same WB pipe-line. More...
|
|
struct | Dss_WbCreateStatus |
| DSS M2M driver create status. Returned after calling Fvid2_create(). More...
|
|
struct | Dss_PipeCfgParams |
| Structure containing video pipe configuration. This structure is used as an argument to IOCTL_DSS_M2M_SET_PIPE_PARAMS. More...
|
|
struct | Dss_PipeMflagParams |
| Structure containing Video Pipe Mflag Information. This structure is used as an argument to IOCTL_DSS_M2M_SET_PIPE_MFLAG_PARAMS. More...
|
|
struct | Dss_PipeCscParams |
| Structure containing Video Pipe CSC Information. This structure is used as an argument to IOCTL_DSS_M2M_SET_PIPE_CSC_COEFF. More...
|
|
◆ Dss_m2mCreateParamsInit()
◆ Dss_m2mPipeCfgParamsInit()
◆ Dss_m2mMFlagParamsInit()
◆ Dss_m2mStatusInit()
Dss_WbStatus structure init function.
- Parameters
-
- Returns
- None