PDK API Guide for J721E
|
DSS Display Write-back Driver interface file.
Go to the source code of this file.
Data Structures | |
struct | Dss_WbPipeCfgParams |
Structure containing video write-back pipe configuration. More... | |
struct | Dss_WbPipeMflagParams |
Structure containing Video write-back Pipe Mflag Information. This structure is used as an argument to IOCTL_DSS_M2M_SET_WB_PIPE_MFLAG_PARAMS. More... | |
struct | Dss_WbStatus |
Structure containing current status of the display M2M driver. This structure is used as an argument to IOCTL_DSS_M2M_GET_CURRENT_STATUS. More... | |
struct | Dss_WbCreateParams |
Structure containing display driver create arguments, used when calling Fvid2_create(). Application shall maintain same create time configurations between multiple driver handles for same WB pipe-line. More... | |
struct | Dss_WbCreateStatus |
DSS M2M driver create status. Returned after calling Fvid2_create(). More... | |
struct | Dss_PipeCfgParams |
Structure containing video pipe configuration. This structure is used as an argument to IOCTL_DSS_M2M_SET_PIPE_PARAMS. More... | |
struct | Dss_PipeMflagParams |
Structure containing Video Pipe Mflag Information. This structure is used as an argument to IOCTL_DSS_M2M_SET_PIPE_MFLAG_PARAMS. More... | |
struct | Dss_PipeCscParams |
Structure containing Video Pipe CSC Information. This structure is used as an argument to IOCTL_DSS_M2M_SET_PIPE_CSC_COEFF. More... | |
Macros | |
#define | IOCTL_DSS_M2M_SET_WB_PIPE_PARAMS (DSS_M2M_IOCTL_BASE + 0x0001U) |
Command to set DSS display M2M pipeline parameters. More... | |
#define | IOCTL_DSS_M2M_SET_WB_PIPE_MFLAG_PARAMS (DSS_M2M_IOCTL_BASE + 0x0002U) |
Command to set MFLAG parameters for WB pipe. More... | |
#define | IOCTL_DSS_M2M_GET_CURRENT_STATUS (DSS_M2M_IOCTL_BASE + 0x0003U) |
Command to get the display status. More... | |
#define | IOCTL_DSS_M2M_SET_WB_PIPE_CSC_COEFF (DSS_M2M_IOCTL_BASE + 0x0004U) |
Command to program the CSC coefficients for WB Pipe. By default BT 601 coefficients are set. More... | |
#define | IOCTL_DSS_M2M_SET_WB_PIPE_DMA_CFG (DSS_M2M_IOCTL_BASE + 0x0005U) |
Command to program the write-back pipe DMA configuration parameters. More... | |
#define | IOCTL_DSS_M2M_SET_PIPE_PARAMS (DSS_M2M_IOCTL_BASE + 0x0006U) |
Command to set DSS display pipeline parameters. More... | |
#define | IOCTL_DSS_M2M_SET_PIPE_MFLAG_PARAMS (DSS_M2M_IOCTL_BASE + 0x0007U) |
Command to set MFLAG parameters for video pipe. More... | |
#define | IOCTL_DSS_M2M_SET_PIPE_CSC_COEFF (DSS_M2M_IOCTL_BASE + 0x0008U) |
Command to program the CSC coefficients for Video Pipe. By default BT 601 coefficients are set. More... | |
Functions | |
static void | Dss_m2mCreateParamsInit (Dss_WbCreateParams *createParams) |
Dss_WbCreateParams structure init function. More... | |
static void | Dss_m2mPipeCfgParamsInit (Dss_WbPipeCfgParams *cfgParams) |
Dss_WbPipeCfgParams structure init function. More... | |
static void | Dss_m2mMFlagParamsInit (Dss_WbPipeMflagParams *mFlagParams) |
Dss_WbPipeMflagParams structure init function. More... | |
static void | Dss_m2mStatusInit (Dss_WbStatus *status) |
Dss_WbStatus structure init function. More... | |