User-provided memory fence call-back function to perform memory sync operations. The operation to perform depends on the opsType flag and also on the CPU/cache architecture.
This function is called after a memory write is performed or before any memory read is performed. In case of write, the ringacc API function needs to insure the write has landed in memory before proceeding. In case of read, the ringacc API function needs to insure the read will land in the memory before proceeding.
- Parameters
-
pVirtAddr | [IN] The virtual memory address written to |
size | [IN] Number of bytes to writeback |
opsType | [IN] CSL_RingAccMemoryOpsType |
- Returns
- None