![]() |
PDK API Guide for J721E
|
CSL_RingAccCfg contains information to configure the ring accelerator.
Data Fields | |
CSL_ringacc_gcfgRegs * | pGlbRegs |
CSL_ringacc_cfgRegs * | pCfgRegs |
CSL_ringacc_rtRegs * | pRtRegs |
CSL_ringacc_monitorRegs * | pMonRegs |
CSL_ringacc_fifosRegs * | pFifoRegs |
CSL_ringacc_iscRegs * | pIscRegs |
uint32_t | maxRings |
uint32_t | maxMonitors |
bool | bTraceSupported |
CSL_ringacc_gcfgRegs* CSL_RingAccCfg::pGlbRegs |
Pointer to Global configuration registers
CSL_ringacc_cfgRegs* CSL_RingAccCfg::pCfgRegs |
Pointer to Configuration registers
CSL_ringacc_rtRegs* CSL_RingAccCfg::pRtRegs |
Pointer to Real-time configuration registers
CSL_ringacc_monitorRegs* CSL_RingAccCfg::pMonRegs |
Pointer to Monitor configuration registers
CSL_ringacc_fifosRegs* CSL_RingAccCfg::pFifoRegs |
Pointer to FIFO registers
CSL_ringacc_iscRegs* CSL_RingAccCfg::pIscRegs |
Pointer to ISC registers
uint32_t CSL_RingAccCfg::maxRings |
Maximum number of rings supported in this ring accelerator configuration
uint32_t CSL_RingAccCfg::maxMonitors |
Maximum number of monitors supported in this ring accelerator configuration
bool CSL_RingAccCfg::bTraceSupported |
Indicates if trace functionality is supported in this ring accelerator configuration