===========================================================================
◆ CSL_RINGACC_MAX_RINGS
#define CSL_RINGACC_MAX_RINGS (1024U) |
Maximum number of rings across devices
◆ CSL_RINGACC_MAX_MONITORS
#define CSL_RINGACC_MAX_MONITORS (64U) |
Maximum number of monitors across devices
◆ CSL_RINGACC_MAX_MONITOR_INTRS
#define CSL_RINGACC_MAX_MONITOR_INTRS (32U) |
Maximum number of monitor interrupts across devices
◆ CSL_RINGACC_CRED_PASSTHRU
#define CSL_RINGACC_CRED_PASSTHRU (0xFFFFFFFFU) |
Bypass credential setting
◆ CSL_RINGACC_ORDERID_BYPASS
#define CSL_RINGACC_ORDERID_BYPASS (0xFFFFFFFFU) |
◆ CSL_RINGACC_RING_EVENT_DISABLE
#define CSL_RINGACC_RING_EVENT_DISABLE (0xFFFFU) |
Macro to pass to disable event
◆ CSL_RINGACC_RING_MODE_RING
#define CSL_RINGACC_RING_MODE_RING ((uint32_t) 0U) |
Exposed ring mode for SW direct access
◆ CSL_RINGACC_RING_MODE_MESSAGE
#define CSL_RINGACC_RING_MODE_MESSAGE ((uint32_t) 1U) |
Messaging mode (all operations are through bus accesses) allowing multiple producers or consumers
◆ CSL_RINGACC_RING_MODE_CREDENTIALS
#define CSL_RINGACC_RING_MODE_CREDENTIALS ((uint32_t) 2U) |
Credentials mode is message mode plus stores credentials with each message. This mode requires each operation to use 2 elements of storage since the credentials are stored in the second element, so the element count should be doubled. Any exposed memory should be protected by a firewall from unwanted access.
◆ CSL_RINGACC_RING_MODE_QM
#define CSL_RINGACC_RING_MODE_QM ((uint32_t) 3U) |
Queue manager mode makes the ring act like a traditional queue manager queue. This takes the credentials mode and adds packet length per element, along with additional read only fields for element count and accumulated queue length. The QM mode only operates with an 8 byte element size (any other element size is illegal), and like in credentials mode each operation uses 2 element slots to store the credentials and length fields.
◆ CSL_RINGACC_RING_MODE_INVALID
#define CSL_RINGACC_RING_MODE_INVALID ((uint32_t) 4U) |
◆ CSL_RINGACC_MONITOR_DATA_SRC_ELEMENT_CNT
#define CSL_RINGACC_MONITOR_DATA_SRC_ELEMENT_CNT ((uint32_t) 0U) |
Monitor the queue element count
◆ CSL_RINGACC_MONITOR_DATA_SRC_HEAD_PKT_SIZE
#define CSL_RINGACC_MONITOR_DATA_SRC_HEAD_PKT_SIZE ((uint32_t) 1U) |
Monitor the packet size at the head of a queue
◆ CSL_RINGACC_MONITOR_DATA_SRC_ACCUM_QUEUE_SIZE
#define CSL_RINGACC_MONITOR_DATA_SRC_ACCUM_QUEUE_SIZE ((uint32_t) 2U) |
Monitor the accumulated data (in bytes) in a queue
◆ CSL_RINGACC_MONITOR_DATA_SRC_INVALID
#define CSL_RINGACC_MONITOR_DATA_SRC_INVALID ((uint32_t) 3U) |
◆ CSL_RINGACC_MONITOR_TYPE_DISABLED
#define CSL_RINGACC_MONITOR_TYPE_DISABLED ((uint32_t) 0U) |
◆ CSL_RINGACC_MONITOR_TYPE_STATS
#define CSL_RINGACC_MONITOR_TYPE_STATS ((uint32_t) 1U) |
Monitor tracks simple statistics on the queue operations. The first value is the count of the number of writes to the queue, and the second value is the count of the number of reads from the queue.
◆ CSL_RINGACC_MONITOR_TYPE_THRESHOLD
#define CSL_RINGACC_MONITOR_TYPE_THRESHOLD ((uint32_t) 2U) |
Monitor uses a programmed low threshold value and a programmed high threshold value to track the data source in the queue and cause an interrupt or status when a threshold is broken, either below the low value or above the high value
◆ CSL_RINGACC_MONITOR_TYPE_WATERMARK
#define CSL_RINGACC_MONITOR_TYPE_WATERMARK ((uint32_t) 3U) |
Monitor tracks the low and high values of the data source since the last read of the monitor
◆ CSL_RINGACC_MONITOR_TYPE_STARVATION
#define CSL_RINGACC_MONITOR_TYPE_STARVATION ((uint32_t) 4U) |
Monitor tracks the number of starvation events (a read to an empty queue) that occurred on the queue
◆ CSL_RINGACC_MONITOR_TYPE_INVALID
#define CSL_RINGACC_MONITOR_TYPE_INVALID ((uint32_t) 5U) |
◆ CSL_RINGACC_MEM_OPS_TYPE_WR
#define CSL_RINGACC_MEM_OPS_TYPE_WR ((uint32_t) 0U) |
◆ CSL_RINGACC_MEM_OPS_TYPE_RD
#define CSL_RINGACC_MEM_OPS_TYPE_RD ((uint32_t) 1U) |
◆ CSL_RingAccRingMode
◆ CSL_RingAccMonitorDataSrc
◆ CSL_RingAccMonitorType
◆ CSL_RingAccMemoryOpsType