PDK API Guide for J721E
|
CSITX Driver configuration file.
Go to the source code of this file.
Macros | |
#define | CsitxTrace |
Log enable for CSITX module. More... | |
#define | CSITX_DRV_ENABLE_DEBUG (1U) |
Enable logging for debug purpose. Set to '1' to enable debug logging. More... | |
#define | CSITX_DRV_LOG_CNT (100U) |
Number of entries to log for debug. More... | |
CSITX Create Default configurations. | |
Default values for create time parameters. See Csitx_CreateParams for details | |
#define | CSITX_NUM_CH (4U) |
Number of Channels: Maximum number of channels for configuration Application can save some memory by reducing this to actual number of channels used rather than all available channels. More... | |
#define | CSITX_CH_ID_DEFAULT ((uint32_t) 0x00U) |
Channel ID: Default channel ID used for initialization. More... | |
#define | CSITX_VC_NUM_DEFAULT ((uint32_t) 0x00U) |
Virtual Channel ID: Default virtual channel ID used for initialization. More... | |
#define | CSITX_OUT_DT_DEFAULT (FVID2_CSI2_DF_RAW12) |
Frame DT: Default frame DT used for initialization. More... | |
#define | CSITX_IN_FRAME_WIDTH_DEFAULT (1920U) |
Frame Width: Default frame width used for initialization. More... | |
#define | CSITX_IN_FRAME_HEIGHT_DEFAULT (1080U) |
Frame Height: Default frame height used for initialization. More... | |
#define | CSITX_IN_FRAME_HB_DEFAULT (0U) |
Horizontal Blanking: Default HB (in terms of number of pixels) used for initialization. More... | |
#define | CSITX_IN_FRAME_VB_DEFAULT (0U) |
Vertical Blanking: Default VB (in terms of number of pixels) used for initialization. More... | |
#define | CSITX_TX_QUEUE_DEPTH_PER_CH ((uint32_t)10U) |
Default max number of frames that can be queued per capture driver instance. More... | |
#define | CSITX_TIMEOUT_VAL_MS ((uint32_t)10U) |
Time out value: Time-out value in ms. This is used as time-out for some of the blocking calls like completion of reset to prevent the driver from hang. More... | |
#define | CSITX_DRV_ENABLE_EXTENDED_DT (1U) |
Extended Data-type support for v2.0 partial support. Set to '1' to enable. More... | |
#define | CSITX_DRV_ENABLE_LS_LE (0U) |
Line Start and Line End packets transmit support. Set to '1' to enable. More... | |