|
PDK API Guide for J721E
|
Go to the documentation of this file. 75 #define CSITX_NUM_CH (4U) 77 #define CSITX_CH_ID_DEFAULT ((uint32_t) 0x00U) 80 #define CSITX_VC_NUM_DEFAULT ((uint32_t) 0x00U) 82 #define CSITX_OUT_DT_DEFAULT (FVID2_CSI2_DF_RAW12) 84 #define CSITX_IN_FRAME_WIDTH_DEFAULT (1920U) 86 #define CSITX_IN_FRAME_HEIGHT_DEFAULT (1080U) 89 #define CSITX_IN_FRAME_HB_DEFAULT (0U) 92 #define CSITX_IN_FRAME_VB_DEFAULT (0U) 95 #define CSITX_TX_QUEUE_DEPTH_PER_CH ((uint32_t)10U) 99 #define CSITX_TIMEOUT_VAL_MS ((uint32_t)10U) 102 #define CSITX_DRV_ENABLE_EXTENDED_DT (1U) 105 #define CSITX_DRV_ENABLE_LS_LE (0U) 110 #define CsitxTrace ((uint32_t) GT_INFO |\ 111 (uint32_t) GT_TraceState_Enable) 115 #define CSITX_DRV_ENABLE_DEBUG (1U) 117 #define CSITX_DRV_LOG_CNT (100U)