PDK API Guide for J721E
|
Capture driver create arguments, used when calling Fvid2_create(). Structure containing Streams configurations.
Data Fields | |
uint32_t | numCh |
Csitx_ChCfg | chCfg [CSITX_NUM_CH] |
Csitx_InstCfg | instCfg |
uint32_t Csitx_CreateParams::numCh |
Number of channels to be configured/processed It should be less that 'CSITX_NUM_CH'.
Csitx_ChCfg Csitx_CreateParams::chCfg[CSITX_NUM_CH] |
Configuration for channels to be processed
Csitx_InstCfg Csitx_CreateParams::instCfg |
CSI Tx module configuration. See Csitx_InstCfg for details