PDK API Guide for J721E
|
CSIRX Low Level Driver SOC specific file.
Go to the source code of this file.
Data Structures | |
struct | Csirx_DPhyCfg |
D-PHY configuration structure. More... | |
Macros | |
#define | CSIRX_NUM_VIRTUAL_CONTEXT (8U) |
CSIRX DRV Virtual Context: Number of virtual contexts per CSI RX port. More... | |
#define | CSIRX_NUM_STREAM (1U) |
CSIRX DRV Numbers: Number of stream per CSI RX module. More... | |
#define | CSIRX_CORE_PIXEL_OUTPUT_BUS_WIDTH (32U) |
Output bus width from CSIRX core in bits. More... | |
CSIRX Module Instance ID | |
#define | CSIRX_INSTANCE_ID_0 ((uint32_t) 0x0U) |
CSIRX Module Instance ID: CSI2RX Module 0. More... | |
#define | CSIRX_INSTANCE_ID_1 ((uint32_t) 0x1U) |
CSIRX Module Instance ID: CSI2RX Module 1. More... | |
#define | CSIRX_INSTANCE_ID_MAX ((uint32_t) 0x2U) |
Maximum value of CSIRX Module Instance. More... | |
CSIRX SoC integration details | |
#define | CSIRX_NUM_STRMS_CAPT ((uint32_t) 2U) |
Total number of capture processing streams available in the SoC. More... | |
#define | CSIRX_NUM_STRMS_OTF ((uint32_t) 1U) |
Total number of OTF(VP/VISS) streams available in the SoC. Note: OTF stream is only supported on 'CSIRX_INSTANCE_ID_0' only. More... | |
#define | CSIRX_NUM_STRMS_LPBK ((uint32_t) 2U) |
Total number of Loop-back streams available in the SoC. More... | |
#define | CSIRX_NUM_CH_CAPT ((uint32_t) 32U) |
Number of capture channels per CSIRX instance. More... | |
#define | CSIRX_NUM_CH_CAPT_MAX |
Number of capture channels that can run in parallel in the SoC. More... | |
#define | CSIRX_NUM_CH_OTF_MAX ((uint32_t) 1U) |
Number of OTF channels that can run in parallel in the SoC. More... | |
#define | CSIRX_NUM_CH_LPBK_MAX ((uint32_t) 1U) |
Number of Loop-back channels that can run in parallel in the SoC. Note: Though each CSI instance have one loop-back stream, only one can be used in the SoC which can be configured on any instance. More... | |
#define | CSIRX_NUM_CH_MAX |
Maximum number of channels that can be processed per CSIRX module These many valid channel configurations can exists per CSIRX DRV instance. More... | |
#define | CSIRX_CAPT_DATA_LANES_MAX ((uint32_t)4U) |
Defines total number of physical data lanes that can be used per CSIRX instance. More... | |
CSIRX D-PHY lane band speed | |
#define | CSIRX_LANE_BAND_SPEED_80_TO_100_MBPS ((uint32_t) 0x00U) |
Lane Band Speed: 80 Mbps to 100 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_100_TO_120_MBPS ((uint32_t) 0x01U) |
Lane Band Speed: 100 Mbps to 120 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_120_TO_160_MBPS ((uint32_t) 0x02U) |
Lane Band Speed: 120 Mbps to 160 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_160_TO_200_MBPS ((uint32_t) 0x03U) |
Lane Band Speed: 160 Mbps to 200 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_200_TO_240_MBPS ((uint32_t) 0x04U) |
Lane Band Speed: 200 Mbps to 240 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_240_TO_280_MBPS ((uint32_t) 0x05U) |
Lane Band Speed: 240 Mbps to 280 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_280_TO_320_MBPS ((uint32_t) 0x06U) |
Lane Band Speed: 280 Mbps to 320 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_320_TO_360_MBPS ((uint32_t) 0x07U) |
Lane Band Speed: 320 Mbps to 360 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_360_TO_400_MBPS ((uint32_t) 0x08U) |
Lane Band Speed: 360 Mbps to 400 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_400_TO_480_MBPS ((uint32_t) 0x09U) |
Lane Band Speed: 400 Mbps to 480 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_480_TO_560_MBPS ((uint32_t) 0x0AU) |
Lane Band Speed: 480 Mbps to 560 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_560_TO_640_MBPS ((uint32_t) 0x0BU) |
Lane Band Speed: 560 Mbps to 640 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_640_TO_720_MBPS ((uint32_t) 0x0CU) |
Lane Band Speed: 640 Mbps to 720 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_720_TO_800_MBPS ((uint32_t) 0x0DU) |
Lane Band Speed: 720 Mbps to 800 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_800_TO_880_MBPS ((uint32_t) 0x0EU) |
Lane Band Speed: 800 Mbps to 880 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_880_TO_1040_MBPS ((uint32_t) 0x0FU) |
Lane Band Speed: 880 Mbps to 1040 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_1040_TO_1200_MBPS ((uint32_t) 0x10U) |
Lane Band Speed: 1040 Mbps to 1200 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_1200_TO_1350_MBPS ((uint32_t) 0x11U) |
Lane Band Speed: 1200 Mbps to 1350 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_1350_TO_1500_MBPS ((uint32_t) 0x12U) |
Lane Band Speed: 1350 Mbps to 1500 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_1500_TO_1750_MBPS ((uint32_t) 0x13U) |
Lane Band Speed: 1500 Mbps to 1750 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_1750_TO_2000_MBPS ((uint32_t) 0x14U) |
Lane Band Speed: 1750 Mbps to 2000 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_2000_TO_2250_MBPS ((uint32_t) 0x15U) |
Lane Band Speed: 2000 Mbps to 2250 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_2250_TO_2500_MBPS ((uint32_t) 0x16U) |
Lane Band Speed: 2250 Mbps to 2500 Mbps. More... | |
#define | CSIRX_LANE_BAND_SPEED_RESERVED ((uint32_t) 0x17U) |
Lane Band Speed: Reserved. More... | |
Functions | |
static void | Csirx_initDPhyCfg (Csirx_DPhyCfg *dphyCfg) |
Csirx_DPhyCfg structure init function. Called through 'IOCTL_CSIRX_SET_DPHY_CONFIG' IOCTL. More... | |
void | CsirxDrv_dphyrxWrapPsmClockConfig (uint32_t addr, uint32_t value) |
void | CsirxDrv_dphyrxCorePpiClockConfig (uint32_t addr, const Csirx_DPhyCfg *dphyCfg) |
void | CsirxDrv_dphyrxCoreLaneReady (uint32_t addr, uint32_t numLanes) |
void | CsirxDrv_dphyrxCoreCommonReady (uint32_t addr) |
int32_t | CsirxDrv_checkDphyrxConfig (const Csirx_DPhyCfg *programmedCfg, const Csirx_DPhyCfg *newCfg) |