PDK API Guide for J721E
|
Multi-Channel SPI driver interface.
============================================================================
The MCSPI header file should be included in an application as follows:
Go to the source code of this file.
Data Structures | |
struct | MCSPI_Params |
MCSPI Parameters. More... | |
struct | MCSPI_FxnTable |
The definition of a MCSPI function table that contains the required set of functions to control a specific MCSPI driver implementation. More... | |
struct | MCSPI_Config |
MCSPI Global configuration. More... | |
Macros | |
#define | MCSPI_MAX_NUM_INSTANCES (SPI_MAX_CONFIG_CNT) |
Max number of MCSPI peripheral instances. More... | |
#define | MCSPI_MAX_NUM_CHANNELS (4U) |
Max number of channels of a MCSPI peripheral instance. More... | |
Typedefs | |
typedef struct MCSPI_Config_s * | MCSPI_Handle |
A handle that is returned from a MCSPI_open() call. More... | |
typedef void(* | MCSPI_CallbackFxn) (MCSPI_Handle handle, SPI_Transaction *transaction) |
The definition of a callback function used by the MCSPI driver when used in SPI_MODE_CALLBACK. More... | |
typedef void(* | MCSPI_CloseFxn) (MCSPI_Handle handle) |
A function pointer to a driver specific implementation of MCSPI_close(). More... | |
typedef int32_t(* | MCSPI_ControlFxn) (MCSPI_Handle handle, uint32_t cmd, const void *arg) |
A function pointer to a driver specific implementation of MCSPI_control(). More... | |
typedef void(* | MCSPI_InitFxn) (MCSPI_Handle handle) |
A function pointer to a driver specific implementation of MCSPI_init(). More... | |
typedef MCSPI_Handle(* | MCSPI_OpenFxn) (MCSPI_Handle handle, const MCSPI_Params *params) |
A function pointer to a driver specific implementation of MCSPI_open(). More... | |
typedef bool(* | MCSPI_TransferFxn) (MCSPI_Handle handle, SPI_Transaction *transaction) |
A function pointer to a driver specific implementation of MCSPI_transfer(). More... | |
typedef void(* | MCSPI_TransferCancelFxn) (MCSPI_Handle handle) |
A function pointer to a driver specific implementation of MCSPI_transferCancel(). More... | |
typedef MCSPI_Config | MCSPI_config_list[MCSPI_MAX_NUM_INSTANCES][MCSPI_MAX_NUM_CHANNELS] |
Functions | |
void | MCSPI_close (MCSPI_Handle handle) |
Function to close a channel of a SPI peripheral specified by the MCSPI handle. More... | |
int32_t | MCSPI_control (MCSPI_Handle handle, uint32_t cmd, void *arg) |
Function performs implementation specific features on a channel of a SPI peripheral specified by the MCSPI handle. More... | |
void | MCSPI_init (void) |
This function initializes the MCSPI module. More... | |
MCSPI_Handle | MCSPI_open (uint32_t idx, uint32_t channel, MCSPI_Params *params) |
This function opens a given channel of a given MCSPI peripheral. More... | |
void | MCSPI_Params_init (MCSPI_Params *params) |
Function to initialize the MCSPI_Params struct to its defaults. More... | |
bool | MCSPI_transfer (MCSPI_Handle handle, SPI_Transaction *spiTrans) |
Function to perform SPI transactions on a channel of a SPI peripheral specified by the MCSPI handle. More... | |
void | MCSPI_transferCancel (MCSPI_Handle handle) |
Function to cancel SPI transactions on channel of a SPI peripheral specified by the MCSPI handle. More... | |