PDK API Guide for J721E
|
MCSPI Global configuration.
The MCSPI_Config structure contains a set of pointers used to characterize the MCSPI driver implementation.
This structure needs to be defined before calling MCSPI_init() and it must not be changed thereafter.
Data Fields | |
MCSPI_FxnTable const * | fxnTablePtr |
SPI_Handle | handle |
uint32_t | chnNum |
MCSPI_FxnTable const* MCSPI_Config::fxnTablePtr |
Pointer to a table of driver-specific implementations of MCSPI APIs
SPI_Handle MCSPI_Config::handle |
Pointer to a SPI instance specific configuration data object
uint32_t MCSPI_Config::chnNum |
channel number