![]() |
PDK API Guide for J721E
|
PMIC Power Resources Driver Interface file.
Go to the source code of this file.
Data Structures | |
struct | Pmic_PowerResourceCfg_t |
Pmic Power resources control and configuration structure. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_PowerCommonCfg_t |
Power configuration The power control and config structure Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_PowerResourceStat_t |
PMIC power status. The PMIC power and thermal status structure. Note: validParams is input param for all Get APIs. other params except validParams is output param for Get APIs. More... | |
struct | Pmic_PowerThermalCfg_t |
PMIC Power Thermal configuration structure Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_PowerThermalStat_t |
PMIC Power Thermal status structure Note: validParams is input param for all Get APIs. other params except validParams is output param for Get APIs. More... | |
Macros | |
PMIC Power Resources Config Structure Param Bits | |
PMIC Power Resources valid params configuration type for the structure member validParams of Pmic_PowerResourceCfg_t structure | |
#define | PMIC_CFG_REGULATOR_VMON_RV_SEL_VALID (0U) |
validParams value used to set/get to Enable/Disable residual voltage checking for regulator/VMON pin Valid only for VMON1/VMON2/BUCK/LDO More... | |
#define | PMIC_CFG_REGULATOR_BUCK_PLDN_EN_VALID (1U) |
validParams value used to set/get to Enable/Disable output pull-down resistor when BUCK is disabled. Valid only for BUCK regulator More... | |
#define | PMIC_CFG_VMON_EN_VALID (2U) |
validParams value used to set/get to Enable /Disable the Voltage monitor feature Valid only for VMON1/VMON2/VMON of BUCK/VMON of LDO/VMON of VCCA Power Resources More... | |
#define | PMIC_CFG_REGULATOR_BUCK_VOUT_SEL_VALID (3U) |
validParams value used to set/get to Select output voltage register for BUCK Valid only for BUCK regulator More... | |
#define | PMIC_CFG_REGULATOR_BUCK_FPWM_VALID (4U) |
validParams value used to set/get to Select PWM or Auto Mode for BUCK Valid only for BUCK regulator More... | |
#define | PMIC_CFG_REGULATOR_BUCK_PWM_MP_VALID (5U) |
validParams value used to set/get to Select between Multi phase with PWM OR AUTO mode with Automatic phase adding and shedding for BUCK Valid only for BUCK regulator More... | |
#define | PMIC_CFG_REGULATOR_EN_VALID (6U) |
validParams value used to set/get to Enable/Disable the power regulators Valid only for BUCK/LDO regulator More... | |
#define | PMIC_CFG_REGULATOR_LDO_SLOW_RAMP_EN_VALID (7U) |
validParams value used to set/get to Enable/Disable Slow Ramp for LDO Valid only for LDO regulator Valid only for TPS6594x Leo PMIC PG2.0 More... | |
#define | PMIC_CFG_REGULATOR_LDO_BYPASS_MODE_EN_VALID (8U) |
validParams value used to set/get to Select Bypass/Linear Regulator LDO mode Valid only for LDO regulator More... | |
#define | PMIC_CFG_VCCA_PWR_GOOD_LVL_VALID (9U) |
validParams value used to set/get Powergood level for VCCA pin Valid only for VCCA More... | |
#define | PMIC_CFG_VMON_RANGE_VALID (10U) |
validParams value used to set/get to Select OV/UV voltage monitoring range for VMON Valid only for VMON1/VMON2 More... | |
#define | PMIC_CFG_REGULATOR_BUCK_ILIM_VALID (12U) |
validParams value used to set/get Switch peak current limit for BUCK regulator Valid only for BUCK regulator More... | |
#define | PMIC_CFG_REGULATOR_BUCK_VMON_SLEW_RATE_VALID (13U) |
validParams value used to set/get Output voltage slew rate for BUCK/VMON Valid only for VMON1/VMON2/BUCK More... | |
#define | PMIC_CFG_REGULATOR_LDO_PLDN_SEL_VALID (14U) |
validParams value used to set/get to Selects the resistor value for output pull-down resistor for LDO regulator Valid only for LDO regulator More... | |
#define | PMIC_CFG_REGULATOR_LDO_RV_TIMEOUT_SEL_VALID (15U) |
validParams value used to set/get LDO residual voltage check timeout select Valid only for LDO regulator More... | |
#define | PMIC_CFG_PWR_RESOURCE_PG_UV_THRESHOLD_LVL_VALID (16U) |
validParams value used to set/get Power good low threshold level for the power resources Valid for all power resources More... | |
#define | PMIC_CFG_PWR_RESOURCE_PG_OV_THRESHOLD_LVL_VALID (17U) |
validParams value used to set/get Power good high threshold level for the power resources Valid for all power resources More... | |
#define | PMIC_CFG_PWR_RESOURCE_RAIL_GRP_SEL_VALID (18U) |
validParams value used to set/get Rail group selection for the power resources Valid for all power resources More... | |
#define | PMIC_CFG_REGULATOR_VMON_VOLTAGE_SET_VALID (19U) |
validParams value used to set/get Voltage level (For LDO/BUCK)/ Powergood voltage level(For VMON1/VMON2) in mv Valid only for VMON1/VMMON2/BUCK/LDO More... | |
PMIC Power Resources valid param bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_PowerResourceCfg_t structure | |
#define | PMIC_CFG_REGULATOR_VMON_RV_SEL_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_VMON_RV_SEL_VALID) |
#define | PMIC_CFG_REGULATOR_BUCK_PLDN_EN_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_BUCK_PLDN_EN_VALID) |
#define | PMIC_CFG_VMON_EN_VALID_SHIFT (1U << PMIC_CFG_VMON_EN_VALID) |
#define | PMIC_CFG_REGULATOR_BUCK_VOUT_SEL_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_BUCK_VOUT_SEL_VALID) |
#define | PMIC_CFG_REGULATOR_BUCK_FPWM_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_BUCK_FPWM_VALID) |
#define | PMIC_CFG_REGULATOR_BUCK_PWM_MP_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_BUCK_PWM_MP_VALID) |
#define | PMIC_CFG_REGULATOR_EN_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_EN_VALID) |
#define | PMIC_CFG_REGULATOR_LDO_SLOW_RAMP_EN_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_LDO_SLOW_RAMP_EN_VALID) |
#define | PMIC_CFG_REGULATOR_LDO_BYPASS_MODE_EN_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_LDO_BYPASS_MODE_EN_VALID) |
#define | PMIC_CFG_VCCA_PWR_GOOD_LVL_VALID_SHIFT (1U << PMIC_CFG_VCCA_PWR_GOOD_LVL_VALID) |
#define | PMIC_CFG_VMON_RANGE_VALID_SHIFT (1U << PMIC_CFG_VMON_RANGE_VALID) |
#define | PMIC_CFG_REGULATOR_BUCK_ILIM_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_BUCK_ILIM_VALID) |
#define | PMIC_CFG_REGULATOR_BUCK_VMON_SLEW_RATE_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_BUCK_VMON_SLEW_RATE_VALID) |
#define | PMIC_CFG_REGULATOR_LDO_PLDN_SEL_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_LDO_PLDN_SEL_VALID) |
#define | PMIC_CFG_REGULATOR_LDO_RV_TIMEOUT_SEL_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_LDO_RV_TIMEOUT_SEL_VALID) |
#define | PMIC_CFG_PWR_RESOURCE_PG_UV_THRESHOLD_LVL_VALID_SHIFT (1U << PMIC_CFG_PWR_RESOURCE_PG_UV_THRESHOLD_LVL_VALID) |
#define | PMIC_CFG_PWR_RESOURCE_PG_OV_THRESHOLD_LVL_VALID_SHIFT (1U << PMIC_CFG_PWR_RESOURCE_PG_OV_THRESHOLD_LVL_VALID) |
#define | PMIC_CFG_PWR_RESOURCE_RAIL_GRP_SEL_VALID_SHIFT (1U << PMIC_CFG_PWR_RESOURCE_RAIL_GRP_SEL_VALID) |
#define | PMIC_CFG_REGULATOR_VMON_VOLTAGE_SET_VALID_SHIFT (1U << PMIC_CFG_REGULATOR_VMON_VOLTAGE_SET_VALID) |
#define | PMIC_POWER_REGULATOR_ILIM_STAT_VALID_SHIFT (1U << PMIC_POWER_REGULATOR_ILIM_STAT_VALID) |
#define | PMIC_POWER_RESOURCE_UV_STAT_VALID_SHIFT (1U << PMIC_POWER_RESOURCE_UV_STAT_VALID) |
#define | PMIC_POWER_RESOURCE_OV_STAT_VALID_SHIFT (1U << PMIC_POWER_RESOURCE_OV_STAT_VALID) |
#define | PMIC_POWER_VCCA_OV_LVL_STAT_VALID_SHIFT (1U << PMIC_POWER_VCCA_OV_LVL_STAT_VALID) |
PMIC Pmic_PowerCommonCfg_s member configuration type. | |
#define | PMIC_POWER_PGOOD_WINDOW_VALID (0U) |
validParams value used to set/get to Select the type of voltage monitoring for PGOOD signal More... | |
#define | PMIC_POWER_PGOOD_POL_VALID (1U) |
validParams value used to set/get to Select the PGOOD signal polarity More... | |
#define | PMIC_CFG_DEGLITCH_TIME_SEL_VALID (2U) |
validParams value used to set/get Deglitch time select for all power resources Valid only for VMON1/VMON2/VCCA/VMON of LDO/VMON of BUCK power resources Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG1.0 and PG2.0 More... | |
#define | PMIC_SEVERE_ERR_TRIG_VALID (3U) |
validParams value used to set/get to Select the trigger selection for severe Error More... | |
#define | PMIC_OTHER_RAIL_TRIG_VALID (4U) |
validParams value used to set/get to Select the trigger selection for other rail group More... | |
#define | PMIC_SOC_RAIL_TRIG_VALID (5U) |
validParams value used to set/get to Select the trigger selection for soc rail group More... | |
#define | PMIC_MCU_RAIL_TRIG_VALID (6U) |
validParams value used to set/get to Select the trigger selection for mcu rail group More... | |
#define | PMIC_MODERATE_ERR_TRIG_VALID (7U) |
validParams value used to set/get Select the trigger selection for Moderate Error More... | |
PMIC valid params bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_PowerCommonCfg_t structure | |
#define | PMIC_POWER_PGOOD_WINDOW_VALID_SHIFT (1U << PMIC_POWER_PGOOD_WINDOW_VALID) |
#define | PMIC_POWER_PGOOD_POL_VALID_SHIFT (1U << PMIC_POWER_PGOOD_POL_VALID) |
#define | PMIC_CFG_DEGLITCH_TIME_SEL_VALID_SHIFT (1U << PMIC_CFG_DEGLITCH_TIME_SEL_VALID) |
#define | PMIC_SEVERE_ERR_TRIG_VALID_SHIFT (1U << PMIC_SEVERE_ERR_TRIG_VALID) |
#define | PMIC_OTHER_RAIL_TRIG_VALID_SHIFT (1U << PMIC_OTHER_RAIL_TRIG_VALID) |
#define | PMIC_SOC_RAIL_TRIG_VALID_SHIFT (1U << PMIC_SOC_RAIL_TRIG_VALID) |
#define | PMIC_MCU_RAIL_TRIG_VALID_SHIFT (1U << PMIC_MCU_RAIL_TRIG_VALID) |
#define | PMIC_MODERATE_ERR_TRIG_VALID_SHIFT (1U << PMIC_MODERATE_ERR_TRIG_VALID) |
PMIC Power Status Config Structure Param Bits | |
PMIC Power Status valid params configuration type for the structure member validParams of Pmic_PowerResourceStat_t structure. | |
#define | PMIC_POWER_REGULATOR_ILIM_STAT_VALID (0U) |
validParams value used to get output current limit status for LDO and buck regulators More... | |
#define | PMIC_POWER_RESOURCE_UV_STAT_VALID (1U) |
validParams value used to get output under voltage status for LDO/ BUCK and input under voltage status for VCCA/VMON Valid for all power resources More... | |
#define | PMIC_POWER_RESOURCE_OV_STAT_VALID (2U) |
validParams value used to get output over voltage status for LDO/BUCK and input over voltage status for VCCA/VMON Valid for all power resources More... | |
#define | PMIC_POWER_VCCA_OV_LVL_STAT_VALID (3U) |
validParams value used to get voltage level status for VCCA Valid only for VCCA More... | |
PMIC Power Thermal threshold type | |
#define | PMIC_THERMAL_WARN_VALID (1U) |
validParams value used to set/get thermal Warning Threshold temperature value More... | |
#define | PMIC_THERMAL_SHTDWN_VALID (2U) |
validParams value used to set/get Thermal Shutdown Threshold temperature value valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG1.0 and PG2.0 More... | |
PMIC Power Thermal threshold type structure Param Bits shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_PowerThermalCfg_t structure | |
#define | PMIC_THERMAL_WARN_VALID_SHIFT (1U << PMIC_THERMAL_WARN_VALID) |
#define | PMIC_THERMAL_SHTDWN_VALID_SHIFT (1U << PMIC_THERMAL_SHTDWN_VALID) |
PMIC Power Thermal status type | |
#define | PMIC_THERMAL_STAT_WARN_VALID (1U) |
validParams value used to get Thermal warning status More... | |
#define | PMIC_THERMAL_STAT_ORD_SHTDWN_VALID (2U) |
validParams value used to get Orderly Shutdown status More... | |
#define | PMIC_THERMAL_STAT_IMM_SHTDWN_VALID (3U) |
validParams value used to get Immediate Shutdown status More... | |
PMIC Power Thermal status type structure Param Bits shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_PowerThermalStat_t structure | |
#define | PMIC_THERMAL_STAT_WARN_VALID_SHIFT (1U << PMIC_THERMAL_STAT_WARN_VALID) |
#define | PMIC_THERMAL_STAT_ORD_SHTDWN_VALID_SHIFT (1U << PMIC_THERMAL_STAT_ORD_SHTDWN_VALID) |
#define | PMIC_THERMAL_STAT_IMM_SHTDWN_VALID_SHIFT (1U << PMIC_THERMAL_STAT_IMM_SHTDWN_VALID) |
PMIC Power Interrupt selection | |
#define | PMIC_POWER_INTERRUPT_ENABLE (0U) |
#define | PMIC_POWER_INTERRUPT_DISABLE (1U) |
Type of voltage monitoring for PGOOD signal: | |
#define | PMIC_POWER_GOOD_UV_MONITOR_ENABLE (0x0U) |
Only undervoltage is monitored. More... | |
#define | PMIC_POWER_GOOD_UV_OV_MONITOR_ENABLE (0x1U) |
Both undervoltage and overvoltage are monitored. More... | |
PGOOD signal polarity | |
#define | PMIC_POWER_PGOOD_POL_HIGH (0x0U) |
PGOOD signal is high when monitored inputs are valid. More... | |
#define | PMIC_POWER_PGOOD_POL_LOW (0x1U) |
PGOOD signal is low when monitored inputs are valid. More... | |
PMIC Power Trigger selection | |
#define | PMIC_POWER_TRIG_IMM_SHUTDOWN (0U) |
#define | PMIC_POWER_TRIG_ODERLY_SHUTDOWN (1U) |
#define | PMIC_POWER_TRIG_MCU_PWR_ERR (2U) |
#define | PMIC_POWER_TRIG_SOC_PWR_ERR (3U) |
Functions | |
int32_t | Pmic_powerSetPwrResourceCfg (Pmic_CoreHandle_t *pPmicCoreHandle, const uint16_t pwrResource, const Pmic_PowerResourceCfg_t pwrResourceCfg) |
API to set power resources configurations. More... | |
int32_t | Pmic_powerGetPwrResourceCfg (Pmic_CoreHandle_t *pPmicCoreHandle, const uint16_t pwrResource, Pmic_PowerResourceCfg_t *pPwrResourceCfg) |
API to get power resources configurations. More... | |
int32_t | Pmic_powerSetCommonConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_PowerCommonCfg_t powerCommonCfg) |
API to Set Power configuration. More... | |
int32_t | Pmic_powerGetCommonConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_PowerCommonCfg_t *pPowerCommonCfg) |
API to Get Power configuration. More... | |
int32_t | Pmic_powerSetConfigPowerGood (Pmic_CoreHandle_t *pPmicCoreHandle, const uint16_t pgoodSrcSel, const uint8_t pgoodSelType) |
API to Set Power good configuration. More... | |
int32_t | Pmic_powerGetConfigPowerGood (Pmic_CoreHandle_t *pPmicCoreHandle, const uint16_t pgoodSrcSel, uint8_t *pPgoodSelType) |
Get Power good configuration. More... | |
int32_t | Pmic_powerGetPwrRsrcStat (Pmic_CoreHandle_t *pPmicCoreHandle, const uint16_t pwrResource, Pmic_PowerResourceStat_t *pPwrRsrcStatCfg) |
API to get power resources status. More... | |
int32_t | Pmic_powerGetPwrThermalStat (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_PowerThermalStat_t *pPwrThermalStatCfg) |
API to get PMIC die temperature thermal status. More... | |
int32_t | Pmic_powerSetThermalConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_PowerThermalCfg_t thermalThreshold) |
API to configure the thermal temperature threshold level for PMIC. More... | |
int32_t | Pmic_powerGetThermalConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_PowerThermalCfg_t *pThermalThreshold) |
Get the PMIC thermal threshold value function. More... | |
int32_t | Pmic_powerSetPwrRsrcIntr (Pmic_CoreHandle_t *pPmicCoreHandle, const uint16_t pwrResource, const uint8_t intrType, const bool intrEnable) |
API to enable/disable Power interrupt. More... | |
int32_t | Pmic_powerSetIntr (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t intrType, const bool intrEnable) |
API to enable/disable Power interrupt. More... | |