![]() |
PDK API Guide for J721E
|
UDMA channel object.
UDMA channel handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.
Data Fields | |
uint32_t | chType |
Udma_ChPrms | chPrms |
Udma_DrvHandle | drvHandle |
uint32_t | txChNum |
uint32_t | rxChNum |
uint32_t | extChNum |
uint32_t | pdmaChNum |
uint32_t | peerThreadId |
Udma_RingHandle | fqRing |
Udma_RingHandle | cqRing |
Udma_RingHandle | tdCqRing |
struct Udma_RingObj | fqRingObj |
struct Udma_RingObj | cqRingObj |
struct Udma_RingObj | tdCqRingObj |
Udma_FlowHandle | defaultFlow |
struct Udma_FlowObj | defaultFlowObj |
Udma_ChTxPrms | txPrms |
Udma_ChRxPrms | rxPrms |
Udma_ChUtcPrms | utcPrms |
uint32_t | chInitDone |
uint32_t | chOesAllocDone |
uint32_t | trigger |
uint32_t Udma_ChHandle::chType |
UDMA channel type. Refer Udma_ChType.
Udma_ChPrms Udma_ChHandle::chPrms |
Object to store the channel params.
Udma_DrvHandle Udma_ChHandle::drvHandle |
Pointer to global driver handle.
uint32_t Udma_ChHandle::txChNum |
Allocated TX channel number - this is relative channel number from base TX channel. This is valid only when the channel is opened for TX and block copy mode
uint32_t Udma_ChHandle::rxChNum |
Allocated RX channel number - this is relative channel number from base RX channel. This is valid only when the channel is opened for RX and block copy mode
uint32_t Udma_ChHandle::extChNum |
Allocated Ext channel number - this is relative channel number from base External channel. This is valid only when the channel is opened for UTC mode
uint32_t Udma_ChHandle::pdmaChNum |
Allocated peer PDMA channel number. This is valid only when the channel is opened for PDMA mode
uint32_t Udma_ChHandle::peerThreadId |
Peer channel thread ID - this is or'ed with thread offset.
Udma_RingHandle Udma_ChHandle::fqRing |
Free queue ring handle
Udma_RingHandle Udma_ChHandle::cqRing |
Completion queue ring handle For AM64x kind of devices, where there is no seperate Completion queue, this points to fqRing itself.
Udma_RingHandle Udma_ChHandle::tdCqRing |
Teardown completion queue ring handle
struct Udma_RingObj Udma_ChHandle::fqRingObj |
Free queue ring object
struct Udma_RingObj Udma_ChHandle::cqRingObj |
Completion queue ring object Not used for AM64x kind of devices, where there is no seperate Completion queue.
struct Udma_RingObj Udma_ChHandle::tdCqRingObj |
Teardown completion queue ring object Not used for AM64x kind of devices, where teardown function is not present.
Udma_FlowHandle Udma_ChHandle::defaultFlow |
Default flow handle
struct Udma_FlowObj Udma_ChHandle::defaultFlowObj |
Default flow object - Flow ID equal to the RX channel is reserved as the default flow for the channel. This object is used for providing handle to the caller to re-program the default flow using the standard flow API's
Udma_ChTxPrms Udma_ChHandle::txPrms |
TX channel parameter passed during channel config.
Udma_ChRxPrms Udma_ChHandle::rxPrms |
RX channel parameter passed during channel config.
Udma_ChUtcPrms Udma_ChHandle::utcPrms |
UTC channel parameter passed during channel config.
uint32_t Udma_ChHandle::chInitDone |
Flag to set the channel object is init.
uint32_t Udma_ChHandle::chOesAllocDone |
Flag to check if the channel's OES is allocated. This is required because the channel OES is used for chaining as well as for TR event registeration. This allows to check for error when both are requested by user on the same channel
uint32_t Udma_ChHandle::trigger |
Channel trigger used when chaining channels - needed at the time of breaking the chaining