![]() |
PDK API Guide for J721E
|
UDMA flow object.
UDMA flow handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.
Data Fields | |
Udma_DrvHandle | drvHandle |
uint32_t | flowStart |
uint32_t | flowCnt |
uint32_t | flowInitDone |
uint32_t | mappedFlowGrp |
uint32_t | mappedChNum |
Udma_DrvHandle Udma_FlowHandle::drvHandle |
Pointer to global driver handle.
uint32_t Udma_FlowHandle::flowStart |
Flow ID start number.
Note: In case of mapped flow(in devices like AM64x), this indicates the mapped flow idx managed by this flow handle.
uint32_t Udma_FlowHandle::flowCnt |
Number of flow IDs allocated - Contiguos flows are allocated
Note: In case of mapped flow(in devices like AM64x), this will be 1 since only one mapped flow is managed by a flow handle.
uint32_t Udma_FlowHandle::flowInitDone |
Flag to set the flow object is init.
uint32_t Udma_FlowHandle::mappedFlowGrp |
The allocated mapped flow group when channel type is UDMA_CH_TYPE_RX_MAPPED.
This is needed to free the mapped flow.
Refer Udma_MappedRxGrpSoc macro for details about mapped RX flow groups.
For unmapped case, this will be UDMA_MAPPED_GROUP_INVALID
uint32_t Udma_FlowHandle::mappedChNum |
The assigned mapped channel number when channel type is UDMA_CH_TYPE_RX_MAPPED.
This is needed to free the mapped flow.
For unmapped case, this will be UDMA_DMA_CH_INVALID.