![]() |
PDK API Guide for J721E
|
UDMA ring object.
UDMA ring handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.
Data Fields | |
Udma_DrvHandle | drvHandle |
uint16_t | ringNum |
uint32_t | ringInitDone |
uint32_t | mappedRingGrp |
uint32_t | mappedChNum |
Udma_DrvHandle Udma_RingHandle::drvHandle |
Pointer to global driver handle.
uint16_t Udma_RingHandle::ringNum |
Ring number
uint32_t Udma_RingHandle::ringInitDone |
Flag to set the ring object is init.
uint32_t Udma_RingHandle::mappedRingGrp |
The allocated mapped ring group when channel type is UDMA_CH_TYPE_TX_MAPPED or UDMA_CH_TYPE_RX_MAPPED.
This is needed to free the mapped ring.
Refer Udma_MappedTxGrpSoc macro for details about mapped TX ring groups or Udma_MappedRxGrpSoc macro for details about mapped RX ring groups.
For unmapped case, this will be UDMA_MAPPED_GROUP_INVALID
uint32_t Udma_RingHandle::mappedChNum |
The assigned mapped channel number when channel type is UDMA_CH_TYPE_TX_MAPPED or UDMA_CH_TYPE_RX_MAPPED.
This is needed to free the mapped ring.
For unmapped case, this will be UDMA_DMA_CH_INVALID.