8.4. Understanding and updating SDK memory map for J721e

8.4.1. Introduction

Jacinto 7 SOC’s have multiple CPUs all collaborating to realize a given application. For all the different CPUs to co-exist and exchange data between themselves, an integrator needs to partition the common DDR memory among the different CPUs and shared memory regions.

This developer note describes the memory partitions that are needed and their constraints. It also describes a Python based tool which can be used to automate the generation of certain files which are used to build the software for a given memory map

8.4.2. Terminology

The CPU names used on Linux side and RTOS side are slightly different as listed below,

CPU name in RTOS CPU name in Linux
mcu1_0 / mcu1_1 mcu_r5fss0_core0 / mcu_r5fss0_core1
mcu2_0 / mcu2_1 main_r5fss0_core0 / main_r5fss0_core1
mcu3_0 / mcu3_1 main_r5fss1_core0 / main_r5fss1_core1
mpu1 na
c6x_1 c66_0
c6x_2 c66_1
c7x_1 c71_0

Note

In this document we will use RTOS names, unless stated explicitly.

8.4.3. Memory partitions and constraints

The table below shows the various partitions that are needed in a typical Jacinto 7 memory map. Depending on the end applications there can be more or less partitions.

Note

  • All partitions listed below MUST be in the 32b address space i.e between 0x80000000 to 0xFFFFFFFF
  • The 16MB alignment “constraints” are mainly due to in C6x, cache/non-cache granularity.
Partition Constraints Description
mcu1_0 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
mcu1_0 code/data
  • cached on this CPU
Used for holding code/data for this CPU
mcu1_1 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
mcu1_1 code/data
  • cached on this CPU
Used for holding code/data for this CPU
mcu2_0 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
mcu2_0 code/data
  • cached on this CPU
Used for holding code/data for this CPU
mcu2_1 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
mcu2_1 code/data
  • cached on this CPU
Used for holding code/data for this CPU
mcu3_0 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
mcu3_0 code/data
  • cached on this CPU
Used for holding code/data for this CPU
mcu3_1 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
mcu3_1 code/data
  • cached on this CPU
Used for holding code/data for this CPU
c6x_1 <-> linux IPC shared region
  • MUST be 16MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
c6x_1 code/data
  • cached on this CPU
  • MUST not overlap with a 16MB region starting from c6x_1 IPC region
Used for holding code/data for this CPU
c6x_2 <-> linux IPC shared region
  • MUST be 16MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
c6x_2 code/data
  • cached on this CPU
  • MUST not overlap with a 16MB region starting from c6x_2 IPC region
Used for holding code/data for this CPU
c7x_1 <-> linux IPC shared region
  • MUST be 1MB aligned
  • MUST be non-cached on this CPU and Linux
Used for IPC between this CPU and Linux
c7x_1 code/data
  • cached on this CPU
Used for holding code/data for this CPU
RTOS <-> RTOS IPC shared region
  • MUST be 16MB aligned
  • MUST be atleast 32MB
  • MUST be multiple of 16MB
  • MUST be non-cached on all CPUs
Used for IPC between all the RTOS CPUs

The table below lists additional partitions required when using vision_apps and tiovx,

Partition Constraints Description
vision apps remote log memory
  • MUST be 16MB aligned
  • MUST be non-cached at all CPUs
Used to redirect printf from all CPUs to Linux
tiovx object descriptor memory
  • MUST be placed after “vision apps log memory”
  • Total size of “vision apps remote log memory” and this memory MUST be multiple of 16MB
  • MUST be non-cached at all CPUs
Used to hold TI OpenVX object descriptors. Basically acts as meta data shared memory between all OpenVX CPUs
ION shared memory
  • MUST be 16MB aligned
  • MUST be cached at all CPUs
Used to hold large pixel/IO buffers which are to be exchanged between different CPUs

8.4.4. Applying the memory map

The memory map described in previous section needs to be applied in the software to take effect when the software is run. This memory map is applied at multiple places within the software. In this section we list the files in which the memory map is applied. In next section, we describe a tool such that memory map can be specified at one place and then the modifications to different files are generated by the tool.

File type Description Example files
Linux dts, dtso file The various carve outs or memory partitions as seen by Linux are listed here
  • arch/arm64/boot/dts/ti/k3-j721e-vision-apps.dtso
  • arch/arm64/boot/dts/ti/k3-j721e-som-p0.dtsi
Linker command file Defines the memory partitions as seen by a specific RTOS CPU
  • vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/<cpu>/linker_mem_map.cmd
MPU/MMU init files Sets up the different CPU specific MMU/MPU based on defined memory regions
  • vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/<cpu>/r5f_mpu.xs
  • vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/<cpu>/main.c
System init files System init functions where we need to pass memory partition information to different APIs, SW modules
  • vision_apps/apps/basic_demos/app_tirtos/app_mem_map.h
  • vision_apps/apps/basic_demos/app_tirtos/common/app_init.c
  • vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/mpu1/app_init.c

8.4.5. Using PyTI_PSDK_RTOS for generating memory map files

8.4.5.1. Installing PyTI_PSDK_RTOS

  • Make sure python3.x and pip3.x is installed

  • Do below to install PyTI_PSDK_RTOS using pip3

    cd vision_apps/tools/PyTI_PSDK_RTOS
    pip3 install -e . --user
    

8.4.5.2. Using PyTI_PSDK_RTOS

  • An example python script to generate memory is located at below path

    vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/gen_linker_mem_map.py
    
  • To generate the memory map related files do below

    cd vision_apps/apps/basic_demos/app_tirtos/tirtos_linux
    ./gen_linker_mem_map.py
    
  • Executing the script generates below files (paths below relative to vision_apps/apps/basic_demos/app_tirtos/tirtos_linux)

    • Linker command files for various RTOS CPUs

      ./c66x_1/linker_mem_map.cmd
      ./c66x_2/linker_mem_map.cmd
      ./c7x_1/linker_mem_map.cmd
      ./mcu2_0/linker_mem_map.cmd
      ./mcu2_1/linker_mem_map.cmd
      
    • Memory map .h file that is used by various system init, mmu/mpu init functions

      ./app_mem_map.h
      
    • Linux DTS file snippets to copy/paste into linux DTS/DTSO files

      ./k3-j721e-vision_apps.dts
      
    • A human readable html table showing the different memory map sections

      ./system_memory_map.html
      

8.4.5.3. Applying the generated memory map

  • The linker command files

    • The linker command files defines the different memory sections specific to a CPU
    • These names should be used in another .cmd file to place memory sections into the defined memory regions
  • Memory map .h file

    • This defines the various memory segments as C #define values for start address and size of the memory region
    • Include this file in various C files to pass these #define’s as init parameters to various APIs
  • Linux DTS file snippets

    • The instructions to apply the Linux dts file changes are printed when the script is executed
    • Follow the instructions to apply the changes
  • Apply the changes for r5f MPU. This step MUST be done manually as of now.

    • The below sections MUST be made non-cache in R5F MPU config (r5f_mpu.xs)

      APP_LOG_MEM_ADDR         # remote printf shared region
      TIOVX_OBJ_DESC_MEM_ADDR  # OpenVX IPC shared region
      IPC_VRING_MEM_ADDR       # RTOS <-> RTOS IPC shared region
      DDR_MCUx_y_IPC_ADDR      # R5F  <-> Linux IPC shared region
      

8.4.5.4. Constructing the memory map

This section shows how to make your own memory map taking the memory map of vision_apps as an example. See file

vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/gen_linker_mem_map.py
  • Install PyTI_PSDK_RTOS as shown here, Installing PyTI_PSDK_RTOS

  • Create a file say gen_linker_mem_map.py. Recommend to have a folder structure as seen inside vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/

  • Import the python package using

    from ti_psdk_rtos_tools import *
    
  • Define and assign global variables for different memory section base addresses and size’s. Recommend to assign values for addresses and size’s using values relative to some base value. This allows to change one memory section and others get adjusted based on the change.

    Example, below we create a section for mcu2_1 CPU relative to mcu2_0 and within mcu2_1 we create partition such that all fit within 64MB.

    mcu2_1_ddr_ipc_addr = mcu2_0_ddr_addr + mcu2_0_ddr_size;
    mcu2_1_ddr_resource_table_addr = mcu2_1_ddr_ipc_addr + linux_ddr_ipc_size;
    mcu2_1_ddr_addr = mcu2_1_ddr_resource_table_addr + linux_ddr_resource_table_size;
    mcu2_1_ddr_size = 64*MB - (mcu2_1_ddr_addr-mcu2_1_ddr_ipc_addr);
    
  • Using these variables create objects of type MemSection.

    • MemSection can be given a name, a attribute string, memory region address, size and a descriptive comment.

      mcu2_1_ddr_ipc             = MemSection("DDR_MCU2_1_IPC", "RWIX", mcu2_1_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for MCU2_1 for Linux IPC");
      
    • It can also be give a string name used in DTS file. Note, the names given for different CPUs these need to match as given in the example file, since the names are used within linux kernel

      mcu2_1_ddr_ipc.setDtsName("main_r5fss0_core1_dma_memory_region", "r5f-dma-memory");
      
    • In DTS files, the internal memory regions within a CPU are not relavent and only total CPU memory region is needed. Use the concat() function to concat internal regions to make one large memory region, which is used for DTS file.

      mcu2_1_ddr_resource_table  = MemSection("DDR_MCU2_1_RESOURCE_TABLE", "RWIX", mcu2_1_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for MCU2_1 for Linux resource table");
      mcu2_1_ddr                 = MemSection("DDR_MCU2_1", "RWIX", mcu2_1_ddr_addr, mcu2_1_ddr_size, "DDR for MCU2_1 for code/data");
      mcu2_1_ddr_total           = MemSection("DDR_MCU2_1_DTS", "", 0, 0, "DDR for MCU2_1 for all sections, used for reserving memory in DTS file");
      mcu2_1_ddr_total.concat(mcu2_1_ddr_resource_table);
      mcu2_1_ddr_total.concat(mcu2_1_ddr);
      mcu2_1_ddr_total.setDtsName("main_r5fss0_core1_memory_region", "r5f-memory");
      
    • In some cases like the ION heap used as shared memory, we dont want the “no-map” flag in DTS file. Use the function setNoMap() to indicate this

      ddr_shared_mem     = MemSection("DDR_SHARED_MEM"    , "", ddr_shared_mem_addr    , ddr_shared_mem_size    , "Memory for shared memory buffers in DDR");
      ddr_shared_mem.setDtsName("vision_apps_shared_region", "vision_apps_shared-memories");
      ddr_shared_mem.setNoMap(False);
      
  • Once MemSection objects are created, now create MemoryMap objects and add the MemSection objects to it.

    • Create a MemoryMap object one per CPU, this is needed for the CPU specific linker command file

      mcu2_1_mmap = MemoryMap("mcu2_0");
      mcu2_1_mmap.addMemSection( r5f_tcma           );
      mcu2_1_mmap.addMemSection( r5f_tcmb0          );
      mcu2_1_mmap.addMemSection( mcu2_1_ddr_ipc     );
      mcu2_1_mmap.addMemSection( mcu2_1_ddr_resource_table  );
      mcu2_1_mmap.addMemSection( mcu2_1_ddr         );
      mcu2_1_mmap.addMemSection( app_log_mem        );
      mcu2_1_mmap.addMemSection( tiovx_obj_desc_mem );
      mcu2_1_mmap.addMemSection( ipc_vring_mem      );
      mcu2_1_mmap.addMemSection( ddr_shared_mem     );
      
    • Use the function checkOverlap() to make sure you are not overlapping memory section’s by mistake

      mcu2_1_mmap.checkOverlap();
      
    • Create a MemoryMap object for the global memory map .h file

      c_header_mmap = MemoryMap(“Memory Map for C header file”); … c_header_mmap.addMemSection( mcu2_0_ddr_ipc ); c_header_mmap.addMemSection( mcu2_1_ddr_ipc ); … c_header_mmap.checkOverlap();

    • Create a MemoryMap object for DTS file

      dts_mmap = MemoryMap("Memory Map for Linux kernel dts/dtsi file");
      ...
      dts_mmap.addMemSection( mcu2_1_ddr_ipc     );
      dts_mmap.addMemSection( mcu2_1_ddr_total   );
      ...
      dts_mmap.checkOverlap();
      
    • Create a MemoryMap object for HTML table file

      html_mmap = MemoryMap("System Memory Map for Linux+RTOS mode");
      ...
      html_mmap.addMemSection( mcu2_1_ddr_ipc     );
      html_mmap.addMemSection( mcu2_1_ddr_resource_table      );
      ...
      html_mmap.checkOverlap();
      
  • Finally invoke the export() function to generate the various files using the created MemoryMap objects

    LinkerCmdFile(mcu2_1_mmap, "./mcu2_1/linker_mem_map.cmd").export();
    
    HtmlMmapTable(html_mmap, "./system_memory_map.html").export();
    
    CHeaderFile(c_header_mmap, "./app_mem_map.h").export();
    
    DtsFile(dts_mmap, "./k3-j721e-vision_apps.dts").export();
    
  • Execute this python file to generate the files

    ./gen_linker_mem_map.py