7. Data SheetΒΆ
Datasheet section contains performance information about various modules within Processor SDK RTOS Automotive SDK for Jacinto 7.
Important
- This information is NOT included on ti.com public release and is available in the ADDON package for Processor SDK RTOS Automotive SDK for Jacinto 7.
- Users can request access to the ADDON package from here [LINK]
- Once access is granted, users can download the the ADDON package from here [LINK]
- Once the ADDON package is installed, the datasheet can be found here ${PSDKRA_ADDON_PATH}/psdk_rtos_auto/docs/datasheet/index.html