PDK API Guide for J721E
|
Output args for CPSW_ALE_IOCTL_GET_PORT_MACADDR IOCTL command.
Data Fields | |
CpswAle_MacAddrInfo * | macAddr |
uint32_t | addrCount |
uint32_t | totalPortMacAddrCount |
CpswAle_MacAddrInfo* CpswAle_GetPortMacAddrOutArgs::macAddr |
Application provided buffer populated with MAC addresses reachable on the given portNum
uint32_t CpswAle_GetPortMacAddrOutArgs::addrCount |
Number of mac entries stored in provided buffer.Will not exceed CpswAle_GetPortMacAddrInArgs::maxNumAddr
uint32_t CpswAle_GetPortMacAddrOutArgs::totalPortMacAddrCount |
Total number of MAC addresses reachable on given portNum