PDK API Guide for J721E
|
Input args for CPSW_ALE_IOCTL_GET_PORT_MACADDR IOCTL command.
Data Fields | |
uint32_t | portNum |
CpswAle_MacAddrInfo * | macAddr |
uint32_t | maxNumAddr |
uint32_t CpswAle_GetPortMacAddrInArgs::portNum |
Port number for which MAC addresses are being queried
CpswAle_MacAddrInfo* CpswAle_GetPortMacAddrInArgs::macAddr |
Application provided buffer into which MAC addresses will be populated
uint32_t CpswAle_GetPortMacAddrInArgs::maxNumAddr |
Max number of MAC entries that can be stored in provided buffer