This is UDMA driver resource manager related configuration parameters and API
|
file | udma_rm.h |
| UDMA RM related parameters and API.
|
|
Returns the default RM config structure based on instance and core. User can use this API to get the default config and override as per need.
Note: The driver internally uses this same API to init the Udma_RmInitPrms structure in UdmaInitPrms_init API
- Parameters
-
- Returns
- Const pointer to default RM init config Udma_RmInitPrms
int32_t Udma_rmCheckDefaultCfg |
( |
void |
| ) |
|
API to check the default configuration across all instance and cores.
- Returns
- Udma_ErrorCodes